2025-07-04 11:02 PM - last edited on 2025-09-17 1:47 AM by Andrew Neil
Hello All,
I have a camera of 5 MP and optical light engine with display of 1280 x 720 pixels.
Can I run both the peripherals on MIPI interface simultaneously such that the camera content is input/feed is input to optical light engine having display of 1280 x 720 pixels. I am using STM32N647A0. Do we have a running example on STM32N6. I have the N6-DK board. Please suggest and recommend.
Best Regards,
Sakshi
2025-07-18 2:23 AM
Hello @sakshi;
Can I run both the peripherals on MIPI interface simultaneously
Which interface do you want to use DCMIPP?
I recommend you to referring to DCMIPP examples STM32CubeN6/Projects/STM32N6570-DK/Applications/DCMIPP at main · STMicroelectronics/STM32CubeN6 · GitHub may help you starting with camera.
I hope this help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.