STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HardFault went reading flash

This routeen fails on the lineFlash_End_Address() at flash_page.c:87 0x80004e6where line 87 is *DATA_64 = *(__IO uint64_t *)StartPageAddress;_______________________________________________________________________________________uint32_t Flash_End_Add...

PGood.1 by Associate II
  • 730 Views
  • 1 replies
  • 0 kudos

Hello every one I have problems with the ISM43362-M3G-L44 module to receive messages from a mqtt broker. Can somebody help me?

I am writing a library for the ISM43362-M3G-L44 module of the B-L475E-IOT01A, and I have a problem with receiving messages from an MQTT broker, when I ask the first time it works correctly but after the module stops responding , it no longer accepts ...

JArra.1 by Associate
  • 800 Views
  • 0 replies
  • 0 kudos

Resolved! External Oscillator

Hi,I'm using STM32F072C8 controller on custom board. I want to use external ready oscillator instead of using crystal component.So need some information on how to interface external oscillator to STM32 controller and configurations that has to be mad...

BPR by Associate II
  • 2434 Views
  • 2 replies
  • 2 kudos

STM32H745 write to S29GL256S NOR flash - FMC

Hi all,the issue is about a custom board with an STM32H45 and an S29GL256S paralel NOR flashAfter FMC is initialized by the CM7 core as in the attached files, i am able to read the NOR flash ID,  but writing data to the IC does not work, memory brows...

0693W00000AOxIqQAL.png 0693W00000AOx7OQAT.png 0693W00000AOx7EQAT.png
VZolt.1 by Associate II
  • 3482 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.