STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Id hardware in OTP STM32f207

Hi everyone!​I am using 1 piece of hardware that uses an STM32f207igh6 that has a registration number on it (serial). However, every time the STM32 f207 chip is damaged, it is necessary to replace the chip with a new one, so that the registration num...

LKint.1 by Associate II
  • 2676 Views
  • 6 replies
  • 0 kudos

Endian problem on STM32 reading Flash

I am  reading 64bit values from flash uint64_t DATA_read = *(__IO uint64_t *)0x0801E010;Where THE FLASH ADDERSS 0x0801E010 contains 5A5A5A5A 00440040DATA_read value afer this read is 0x400044005a5a5a5aif I read uint64_t DATA_read = *(__IO uint64_t *)...

PGood.1 by Associate II
  • 2824 Views
  • 4 replies
  • 0 kudos

How to get data from a fixed address after startup?

I want to take out the data I need from a certain address after startup, I created an array inside tf-a ( char array [0x200] = {}) , and I read the address of the array printf("%p", (void*) &array), which seems to never be repeated after many...

0693W00000BZbG5QAL.png
DDing.1 by Associate II
  • 1596 Views
  • 2 replies
  • 0 kudos

F042 ADC DMA malfunction:?? I am using a Nucleo_F042k board but will target a F042F MCU later. I'm using DMA to set up 2 ADC channels + the 3 internal ADC values. Results : 1: 2146: 2: 1668: 3: 0: 4: 0: 5: 0. Only the first is verifiable.

I have probably missed something simple. I use CubeMx to Configure the A2D channels hadc.Instance = ADC1; hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1; hadc.Init.Resolution = ADC_RESOLUTION_12B; hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT; ...

DIngr.1 by Associate II
  • 1320 Views
  • 1 replies
  • 0 kudos

about dominant error

Dear Guys I get the "bit dominant error" when programming for can with STM32F302. even i set CAN_MODE_SILENT_LOOPBACK mode , also get this error after exec the statement  "SET_BIT(hcan->Instance->sTxMailBox[transmitmailbox].TIR, CAN_TI0R_TXRQ);" a...

0693W00000BZZg1QAH.png 0693W00000BZZfhQAH.png
kevin xu by Associate II
  • 1655 Views
  • 2 replies
  • 0 kudos

Wrong data through SPI on STM32F7

Hello dear community. I'd tried so long so i decided to ask for you.I need to send some data pack from STM32F7(master) to STM32F1.I use STM32CubeIDE platform. My code is below.Problem is that in receiving back data by master. First byte has always co...

DVovk.1 by Associate II
  • 16924 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.