STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! OS install error

I just got a stm32L475 Iot Kit.And after compilation, I got this error .st-flash 1.7.0-23-ga9adf9c2021-05-21T22:17:24 INFO common.c: L4xx: 96 KiB SRAM, 1024 KiB flash in at least 2 KiB pages.open(./BUILD/DISCO_L475VG_IOT01A/GCC_ARM/thingsboard-l475vg...

KYang.7 by Associate
  • 2076 Views
  • 3 replies
  • 0 kudos

Does ST confirm the LpTimer issue with stop mode?

The LPTIMER OF STM32l0(Config BASED ON LSI) can cause the CPU to be temporarily stuck in the LPTIM ISR with no way for the CPU to clear the IRQ.The bug is well described here with a workaround, can someone from ST confirm this issue, and if there is ...

Resolved! SPI4 error

Hi,I'm trying to use SPI to communicate between two boards. On the MASTER side, i am using the HAL_SPI_Transmit(&hspi4, (uint8_t*)TxData,sizeof(TxData),100); and on the slave side i have enabled the interrupt, HAL_SPI_Receive_IT(&hspi4,RxData,1); The...

IRodr.2 by Associate II
  • 4564 Views
  • 6 replies
  • 0 kudos

Resolved! Extend RAM STM32F429

Hey,I have a discovery board (https://www.st.com/resource/en/data_brief/32f429idiscovery.pdf)This board has an on board 64 MBit SDRAM.Now i have read in other posts that RAM extension is not possible in an SPC line MCU. However what about the STM32F4...

Debugging probe StLink V3. GND Detect input (?) signal. What is the minimal set of connections essential? What about VCC input?

Hello, I connected my probe StLink V3 MODS via only: GND, SwClk, SwDio (CN2.pin8.13,4) for the beginning. And it rather works. Rather as once I got a strange message instead of debugging. I would like to have my probe reliable so I have found that I...

RnnKrk by Associate II
  • 5329 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 , how to set the "analog switch" for _C pins

Dear experts,I'm using Cube to assign pins for my stuff (yep...) and it offers some pins with _C sufix (PC2_C, PC3_C).From the RM0433 fig.75 I gather this is something with the "analog switch" and in order to use these _C pins as AF for some device (...

Pavel A. by Super User
  • 2522 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.