STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L010 and NXP NT3H2211 (I2C question)

Greetings everyone, I am trying to communicate with NT3H2211.My specific problem is marked red on the picture (everything else I manage to successfully send/receive). When reading data NT3H2211 wants to get " 7 bits SA and '1' " and then it will send...

JZida.1 by Associate II
  • 1662 Views
  • 1 replies
  • 0 kudos

Resolved! External Loader for STM32H750VBT6 with NOR Flash(W25Q128JQ)

We have built custom board using STM32H750VBT6.We have tried to make external loader for this MCU with w25q128Jq NOR flash of winbond.Also take one reference project from community which name is SW_H750_QSPI_Ext_LoaderKeil and modified command for NO...

djtilava by Associate II
  • 3062 Views
  • 3 replies
  • 0 kudos

How to select PSRAM compatible with STM32F407 FSMC ?

Hi,There are two points I want to understand them.first one:-I want to use PSRAM with STM32F407 FSMC when I used STM32cubeMX it support Muxed PSRAM only although, STM32F407 reference manual says that it support Multiplexed or nonmultiplexed PSRAM (...

MHass.2 by Associate III
  • 2878 Views
  • 2 replies
  • 0 kudos

Help to use SPI Receivce Only Slave correctly with an ADC

HiI have a project were i should communicate with an AD7768 ADC from my Nucleo-H743ZI2. The AD7768 is setup as SPI master and the stm32H743 is setup in SPI Receive slave only mode.There is three connections between the two devices, a clock signal, a ...

LKris.1 by Associate II
  • 2889 Views
  • 5 replies
  • 0 kudos

Is possible to create a custom bin to gather all the data with a short period time and later show all on the screen using serial COM?

We are testing motor failure detection using the "STEVAL-IDP005V1" sensor in conjunction with the "STEVAL_UKI001V1" card on a core stm32. The idea is to be able to capture all the possible data in a short period of time (5 seconds approx), which is t...

RMedi.3 by Associate
  • 1184 Views
  • 1 replies
  • 0 kudos

QSPI sends wrong instruction

Dear Readers,i try to connect to a LY68L6400 via Quad SPI. I manage without Problems to read the ID of the Chip, which i think means the communication is Working. When i try to write data (by Sending 0x38 as instruction) The instruction is changed to...

About using virtual com ports with STM32F767

Hello!Before I forget, I'm using STM32IDE 1.6.1 on Linux. The board is a custom design. In order to make the problem reproductible, I have reproduced the problem on a Nucleo 144 board with STM32F767.I have setup a VCOM port using USB cdc, and it work...

PG.1 by Associate III
  • 919 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.