STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 CubeMx SPI HAL Driver Initial Pin Level

Hi there, I created a project with STM32F042G6 chip using CubeMX. I am interfacing this IC to another chip using SPI. When I set the SPI1 and try to send a command, just before sending a command I have SCLK, MOSI, and MISO levels are high. After send...

DAkka by Associate
  • 1485 Views
  • 2 replies
  • 0 kudos

STM32H745 Data share

Hi I'm new to dual core programming. I need to share data from M7 core to M4 core and M4 core to M7 core. Can you please let me know the steps I need to start.?

TWalp.1 by Associate II
  • 2978 Views
  • 5 replies
  • 0 kudos

STM32H743ZI2 CAN message receive issue with MCP2551

I have hooked up a STM32H743ZI2 Nucleo board with a CAN tranceiver MCP2551 following the instructions kindly provided by mr. Hudak (https://os.mbed.com/users/hudakz/code/CAN_Hello/) with the exception of replacing the second board with a USB-CAN-modu...

SAmpi.1 by Associate
  • 2818 Views
  • 3 replies
  • 0 kudos

Issue with the STM32H735-DK, OSPI Hyperram

Hi, in the example for the OSPI-memorymapped example, the test procedure is as follows..// This is running fine on the DEV board, ( it also works in byte mode fine.) while (1) { /* Intensive Access ---------------------------------------------...

Naldr.1 by Associate
  • 1770 Views
  • 3 replies
  • 0 kudos

STM32H735 OCTOSPI2 Hyperram Errors

Using the STM32H735G-DK with on board external memory connected to OCTOSPI2.I'm using the demo code for this board to initialise the OSPI2 interface and to access the on board HyperRAM (S70KL1281DABHI023). The demo code writes 32-bits and reads them...

HSamm.1 by Associate II
  • 2117 Views
  • 3 replies
  • 0 kudos

Resolved! Connect segger jlink to STM32H735G-DK discovery board

Hi, I would prefer to use my segger jlink debugger with the discovery board io using stlink. I see there is an unpopulated header with 3V3 , SWCLK, GND, SWDIO on the left side of the board, and there is an NRST pin on the back connectors so I think ...

Use of ADC with DMA

Dear community,In a project the microcontroller STM32G4 is used, where three ADCss with DMA are used. On each ADC three channels are configured with 2.5 cycle sampling. The ADCs are triggered with a timer with a frequency of 125kHz.The processed data...

Garm by Associate
  • 2066 Views
  • 3 replies
  • 0 kudos

Resolved! Reading images from external flash

Hi, I want to store images in external flash (W25Q32) . I did the linker script modifications. But I couldn't find that what should i do after it. Could you help me?EDIT : I think that I need the external loader.

Ezgi by Senior
  • 1265 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.