STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC of STM32L072CZ. DBP=1 needed, to write to RTC->ISR?

I know that the 0xCA 0x53 sequence into RTC->WPR is not needed to write to RTC->ISR (because RTC->ISR is an exception to that 0xCA 0x53 rule) but, is it still needed to set DBP=1 in PWR->CR to write to RTC->ISR?I am not sure if the writability of RT...

I am using STM32F103RGT controller. I want to use the PWM-CH and PWM CHN complementary pwm in my application. I have created 4 PWMs 2 complementary each others. but I could not able make the phase shift.

Dear Team,I want to use the 4 pwms for the phase shifted full bridge application. But I am unable to generate phase shifted pwms. Request to guide how to configure and used the PWMs with phase shifted pwm waveforms from the microcontroller...

DSaha.3 by Associate II
  • 6182 Views
  • 7 replies
  • 0 kudos
hinou.11 by Associate II
  • 1906 Views
  • 8 replies
  • 0 kudos

ads124s08 with STM32F407VGT6 spi communication problem

I need to get information from an ti's ads124s08 and imported an example from arduino forums. I can communicate with device using an arduino for test (on the same board and same specs) but can not use with stm. In fact, i think there should be a prob...

TBala.1 by Associate
  • 3156 Views
  • 2 replies
  • 0 kudos

Self-generated breaks are not detected sometimes

We configured our controller (STM32F427IG) as master and USART8 to LIN-mode. We observed, that the own breaks are detected with the break detection interrupt. Furthermore, we also get the framing error interrupt as the stop bit arrives later for the ...

0693W00000BZxSIQA1.png
TGnäg.1 by Associate II
  • 3690 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.