STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC works sometimes STM32f303RE

Hi.I am having problems with the ADC, for some reason, it only works when I put a breakpoint in the function I use to enable the ADC to debug, but, if I run it without any breakpoint, it does not work.line of code I use to extract a value from the AD...

Data reading fail in external loader

Hi, I wrote an external loader and tested for write, erase sector, erase chip. They all worked but I have a problem about reading. I thought it was because of the verify function in Loader_Src. Can someone explain what the function does?

Ezgi by Senior
  • 901 Views
  • 1 replies
  • 0 kudos

STM32G030 Flash Read/Write issues.

>>Hi I am trying to write and read data from FLASH in STM32G030 32KB Flash device.>>However , I am experiencing unusual behavior . Sometimes I am able to read data correctly and sometimes junk data is read.Following is my code :#define FLASH_USER_STA...

PGand by Associate
  • 2242 Views
  • 2 replies
  • 0 kudos

Resolved! question about timers and.

Hello guys , i am supposed to construct a square wave with automatic toggling making use of the output compare channel one setting. the channel one of the timer is in pin PA6 Does anyone know if this is also the pin were the output (final waveform) w...

0693W00000BaAZgQAN.png
GSant.5 by Associate II
  • 870 Views
  • 1 replies
  • 0 kudos

Hi, I was wondering how would i output to the display that comes with my STM32H747i-disco. I wanted to do a test hello world. What would i need to do to get it working. I have the cube IDE installed and have flashed a test demo program to the screen.

What do i need to do to interface with the display to print a hello world program or to have a shape/ clock appear on the screen. How would i get audio working. I have used arduino/ raspi / and tm4c from ti and I am a bit lost trying to use the stm32...

HSyed.1 by Associate II
  • 1606 Views
  • 2 replies
  • 0 kudos

Reading from IMU at specific frequency

Greetings, I have an i2c connected IMU. I've connected it to a DMA channel and reading/writing like that. However, IMUs have a capability to run at a specific output data rate (ODR). In other architectures I would connect the interrupt pin to an ...

STM32L071CB Ultra Low Power issue with LL libraries

Hello,I'm trying to get my STML071CB down to the lowest possible current, but can't seem to get to the low levels provided int he datasheets with my own code. I'm using the LL libraries and am going into STOP mode using the following code: LL_PWR_En...

DPast.1 by Associate II
  • 1673 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.