STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F3 DMA triggered by ADC triggered by TIM without HAL

Hello,currently I'am working on a STM32 project with the CMSIS core. I want the ADC getting triggered by a Timer (TIM3). Iam trying to do that with the TRGO option.The ADC should sample 4 different channels. Each channel then gets transfered by the D...

MF.3 by Associate
  • 1538 Views
  • 1 replies
  • 0 kudos

Weirdest thing happening with STM32H7 I2S hardware

Hi guys! I am having the biggest issue with the I2S right nowWhat is happening: For whatever reason the I2S does not want to transmit any samples VIA DMA. Doesnt matter what I do what I try.The weird thing happening: The I2S WS, SCLK wont work. Only ...

CLeo.1 by Senior II
  • 6674 Views
  • 25 replies
  • 0 kudos

UART not receiving NULL hex bytes on STM32F103C8T6.

I'm using STM32F103C8T6 processor with an 8MHz internal clock, 9600 baud rate, 8bit + 1stop bit and no parity. For receiving uart data, I'm using a global interrupt. While I'm receiving data with usart1 or usart2, I can not receive null bytes. Now I ...

0693W00000BaCIwQAN.jpg
BJako.1 by Associate II
  • 3257 Views
  • 7 replies
  • 0 kudos

STM32H7 Using SPI with DMA circular mode

Hello,i currently use SPI interface of my STM32H7B3I board with DMA (mode circular) to build up a connection to Raspberry Zero W (using Python spidev-lib).At the beginning, I start HAL_SPI_TransmitReceive_DMA() where the data exchange is initialized....

CKörn.2 by Associate II
  • 4037 Views
  • 6 replies
  • 0 kudos

I want to know the parallel communication

Hello All,If I pass 0x38 hex value into my function, that should be came out from my one of the port as parallel data, how to do this ? please give me a simple example with code and explanation.My youtube channelStm32user

How to unlock STM32F103C8T6 ?

Hello, I have several modules with STM32F103C8T6 (called Blue Pills). But I cannot get them to runthe programs. I can freely write or read flash memory with stm32cubeprogrammer, but there is always warning (even when I want to start the program), tha...

bully by Senior
  • 2326 Views
  • 2 replies
  • 0 kudos

Resolved! Write and read using Flash memory on STM32F7xx (24 sectors)

I've got the following structure to write to memory:```#define FLASH_CONFIG_START_ADDR ((uint32_t) 0x080E0000)#define FLASH_CONFIG_END_ADDR ((uint32_t) 0x080E0040)union NVRAM { Config_t config; uint8_t data[512];} DevNVRAM;```I've used this code for ...

ZYagu.1 by Associate II
  • 8584 Views
  • 14 replies
  • 0 kudos

CLOSED - USART receiver not working on F446RE MCU

Hello all,I'm trying to implement a really simple exercise:Send a char via USART2 (PA2);Receive the char via USART1 (PA10);After the char is received, within an interrupt I increase a variable called "Debug".The only HW connection done is that betwee...

FGiai.1 by Associate II
  • 5888 Views
  • 16 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.