STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Changing EXTINT Trigger Type after Init

Hi All,I'm using the following code to set up 4 external triggers and this all works well. What I'd like to do is to be able to change the trigger type of any of the EXTINT at some point in the program. I've tried a couple of things which only resu...

PSpei by Associate II
  • 5740 Views
  • 3 replies
  • 0 kudos

Advice on STM32F103 GPIO port sharing

First, the "atomic" port ODR issue when more than one function or task may use the same GPIO port. Is the best thing to do ALWAYS to use BRR and/or BSRR to change the ODR values? From what I've read we need to be wary of an interrupt or other task ch...

Grant Bt by Senior II
  • 4964 Views
  • 8 replies
  • 0 kudos

STM32L412CBT6P startup problem

I have soldered MCU chip to a PCB and programed it by ST-Link using STM IDE.when I run MCU using ST-Link it is working fine. But When I use an external DC supply it's showing malfunction, (most of the time not working). I have connected the BOOT0 pin...

Spatr.1 by Associate
  • 921 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F745 FMC SDRAM Interface Theoretical Timining

Hello,I want to setup a STM32F745IEK6 together with an SDRAM from Micron Type MT48LC8M16A2P-6A.I analyzed the theoretical signal Intergrity for the devices and I had to end because of my question:The setup time of MT48L is required with min. 1,5 ns. ...

FGrie.1 by Associate
  • 1231 Views
  • 1 replies
  • 0 kudos

SYSCLOCK configuration problem on STM32F100VE

Hello, I have a software that has been workingfine for several years on a STM32F100VCT6. However, today we are trying to use thissoftware on the MCUs ref: 100VDT6 or 100VET6. On these 2 new references no programming problem with the same binary file....

VCedr.1 by Associate
  • 1771 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.