STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the production status of STM32H75 chips?

I once again checked at Digikey and they had only one of those. Will the rest of them ever come backI would to like have STM32H76x 144 pin lgfp, but it is of no use if there are none available when I finish my PCB.

LMI2 by Lead
  • 852 Views
  • 3 replies
  • 0 kudos

Time base interrupt STM32G4 HAL overflowing?

Hello everyone,this is my first post here, please my apologies if I mistake some terms since we jumped into the ST controller world in the company around 6 months ago and I am still learning about the technologies.I have been working so far on a proj...

0693W00000Bb7UVQAZ.jpg
CMart.8 by Associate
  • 1187 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L4, can't wake up with RTC Alarm A after Stop 2 mode (WFE)

Hi all,As stated above, I can't seem to wake up the controller from STOP2 mode using WFE with the ALARM A. Here's my alarm and EXTI settings:if(EXTI->PR1 & EXTI_PR1_PIF18) { EXTI->PR1 |= EXTI_PR1_PIF18; ///< Clear pending interrupt if necessary } EX...

AFahr.1 by Associate III
  • 2139 Views
  • 5 replies
  • 0 kudos

Resolved! Error in Datasheet Rev.8 of STM32L412CB?

I am developing an application for a STM32L412CB and use the comparator COMP1. I designed my pinout with CubeMX and put the output of the comparator on PB0. I also checked table 14 in the Datasheet Rev.8 on page 58, if it is correct. Now I wanted to ...

Write to external SRAM in four #WE cycles.

Hello!To MCU STM32h743 connected 16-bit SDRAM and 16-bit SRAM. Writin to SRAM uses four #WE cycles in conjunction with BLS0 and BLS1. When write 8 or 16 bits BLS# active only for one #WE cycle, when 32 bits - two cycle and four cycle for 64 bits. I c...

AAshc by Associate
  • 761 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.