cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 vs STM32MP1 for heterogenous application use case

ramkumarkoppu
Senior

For one of the heterogenous application use case, we would like run always-on code in Cortex-M4 and high end application, we have two options. either run Cortex-M7 if se select STM32H7 device or Cortex-A7 if select STM32MP1 device. Assuming that both of these devices allow Cortex-M4 as always-on and high end CPU (either M7 for STM32H7 or A7 for STM32MP1) and ignoring Linux support, which device more energy efficient. is it STM32H7 or STM32MP1?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Christophe Guibout
ST Employee

Hi @ramkumarkoppu​ ,

The article How to define your low-power strategy in STM32MP1 wiki gives some power figures.

Hope it will help.

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.