2021-06-14 7:23 AM
Hi all,
As stated above, I can't seem to wake up the controller from STOP2 mode using WFE with the ALARM A. Here's my alarm and EXTI settings:
if(EXTI->PR1 & EXTI_PR1_PIF18)
{
EXTI->PR1 |= EXTI_PR1_PIF18; ///< Clear pending interrupt if necessary
}
EXTI->EMR1 |= EXTI_EMR1_EM18; ///< RTC Alarm Mask
EXTI->RTSR1 |= EXTI_RTSR1_RT18; ///< Rising trigger
/* Set the alarm values with the config values */
HAL_PWREx_EnableInternalWakeUpLine();
__HAL_RTC_ALARMA_ENABLE(&hrtc);
__HAL_RTC_ALARM_CLEAR_FLAG(&hrtc, RTC_FLAG_ALRAF);
alarm_Time.Hours = storage_config.wup_time.Hours;
alarm_Time.Minutes = storage_config.wup_time.Minutes;
alarm_Time.Seconds = storage_config.wup_time.Seconds;
alarm_Time.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
alrm_a.Alarm = RTC_ALARM_A;
alrm_a.AlarmMask = RTC_ALRMAR_MSK4;
alrm_a.AlarmDateWeekDay = RTC_WEEKDAY_MONDAY;
alrm_a.AlarmTime = alarm_Time;
alrm_a.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;
HAL_RTC_DeactivateAlarm(&hrtc, RTC_ALARM_A);
if (HAL_RTC_SetAlarm(&hrtc, &alrm_a, RTC_FORMAT_BIN) != HAL_OK)
{
log_msg(LOG_ERR, "dg_system.c: Error setting alarm Line: %u", __LINE__);
}
log_msg(LOG_INFTo send the unit to sleep (I'm using FreeRTOS):
/* Send system to sleep */
vTaskSuspendAll();
vPortRaiseBASEPRI();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFE);I know that the code above works, because I can wake up the micro using a push button:
GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_EVT_RISING;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(USB_Det_GPIO_Port, &GPIO_InitStruct);But either I'm not configuring the Alarm correctly or there is some incorrect setting in the EXTI. I cannot really use an interrupt, as the OS would then trigger it...
Any ideas or pointers are welcome.
Cheers,
Alberto
Solved! Go to Solution.
2021-06-14 11:24 PM
Which STM32?
I believe you don't need to enable the interrupt in NVIC and it would suffice to set ALRAIE/ALRBIE in RTC.
JW
2021-06-14 4:23 PM
I seem to again have found my own solution... I had to enable the RTC interrupt even though I'm only using the event.... I get confused by that still.
if(EXTI->PR1 & EXTI_PR1_PIF18)
{
EXTI->PR1 |= EXTI_PR1_PIF18; ///< Clear pending interrupt if necessary
}
EXTI->EMR1 |= EXTI_EMR1_EM18; ///< RTC Alarm Mask
EXTI->RTSR1 |= EXTI_RTSR1_RT18; ///< Rising trigger
/* Set the alarm values with the config values */
HAL_PWREx_EnableInternalWakeUpLine();
__HAL_RTC_ALARMA_ENABLE(&hrtc);
__HAL_RTC_ALARM_CLEAR_FLAG(&hrtc, RTC_FLAG_ALRAF);
alarm_Time.Hours = storage_config.wup_time.Hours;
alarm_Time.Minutes = storage_config.wup_time.Minutes;
alarm_Time.Seconds = storage_config.wup_time.Seconds;
alarm_Time.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
alrm_a.Alarm = RTC_ALARM_A;
alrm_a.AlarmMask = RTC_ALRMAR_MSK4;
alrm_a.AlarmDateWeekDay = RTC_WEEKDAY_MONDAY;
alrm_a.AlarmTime = alarm_Time;
alrm_a.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;
HAL_NVIC_SetPriority(RTC_Alarm_IRQn, 7, 0); ///< Set the interrupt priority and enable
HAL_NVIC_EnableIRQ(RTC_Alarm_IRQn);
HAL_RTC_DeactivateAlarm(&hrtc, RTC_ALARM_A);
if (HAL_RTC_SetAlarm_IT(&hrtc, &alrm_a, RTC_FORMAT_BIN) != HAL_OK)
{
log_msg(LOG_ERR, "dg_system.c: Error setting alarm Line: %u", __LINE__);
}
log_msg(LOG_INFO, "Setting alarm: %02d:%02d:%02d", alrm_a.AlarmTime.Hours, alrm_a.AlarmTime.Minutes, alrm_a.AlarmTime.Seconds);This worked when I turned it off at 11 PM and it woke up at 6 AM again.
Cheers,
Alberto
2021-06-14 11:24 PM
Which STM32?
I believe you don't need to enable the interrupt in NVIC and it would suffice to set ALRAIE/ALRBIE in RTC.
JW
2021-06-14 11:26 PM
Thanks Jan,
I will give that a try.
It's an STM32L496
Cheers,
Alberto
2021-06-15 9:40 PM
@Community member Hi, you were right, enabling the ALRAIE bit did the trick, no need to enable the interrupt!
Cheers,
Alberto
2021-06-16 4:50 AM
Hello @Community member,
In order to help other users found quickly the solution please mark waclawek.jan's answer as Best.
Thanks,
Mohamed Aymen.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.