STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Failed to communicate with device using Nucleo uart

Hello,I'm using nucleo board f410rb to communicate with another device via UART, my Baudrate is correctly fixed , i checked with the builder of the device the command i should send , i wrote the following code but the device dosen't respond uint8_t t...

Ahajr.1 by Associate II
  • 1358 Views
  • 1 replies
  • 0 kudos

Resolved! Translating incoming data from PA10 (USART1 Rx) to PB4 (JTRST) with erased FLASH or under reset in STM32G473

I have RS-485 transceiver connected to USART1 (PA9 + PA10) and relay connected to PB4. If MCU have erased FLASH or RST-pin connected to GND all incoming data to pin PA10 (Rx) for RS-485 line translated to pin PB4 in inversion (0 on PA10 => 1 on PB4, ...

Nabekaite by Associate II
  • 3521 Views
  • 8 replies
  • 0 kudos

Not able to program STM32F407G-DISC1 via onboard ST-LINK. In STM32CubeProgrammer Target voltage is detected as 0.

I purchased a new STM32F407G-DISC1 (MB 997D) board last week. As shown in many of the videos, I am not able to program it using STM32CubeIDE. Tried with ST-Link utility & STM32CubeProgrammer as well but no luck. I observed target voltage is detected ...

nilesh-g by Associate
  • 1592 Views
  • 2 replies
  • 0 kudos

STM32L412 and reference voltage buffer

STM32L412xx datasheet DS12469 even in Rev. 8 talks about � Accurate 2.5 V or 2.048 V reference voltage buffered outputon the front page. The reference manual gives only availability on L43 and L45.

Powering STM32 L476RG at 1.8V - Any major disadvantages?

I'm currently using the STM32 L476RG for an application where I need to communicate with peripherals through SPI at 1.8V. Currently I'm using the TXB0108 bidirectional logic level shifter to convert my SPI lines from 3.3V to 1.8V but there are proble...

LBouz.1 by Associate II
  • 1571 Views
  • 3 replies
  • 0 kudos

Corrupted data via SPI_HAL_Receive in STM32F407

Dear friends, I need your help with the issue of data corruption when reading the data on SPI bus in STM32F407. I'm using 24 channels of temperature measurement (slaves) with one master STM32F407. 12 channels are connected to SPI1, other 12 channels ...

OVeli.1 by Associate II
  • 2375 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.