2021-06-17 1:02 AM
Hello,
I'm using nucleo board f410rb to communicate with another device via UART, my Baudrate is correctly fixed , i checked with the builder of the device the command i should send , i wrote the following code but the device dosen't respond
uint8_t tx_buff[]={0x02, 0x00, 0x08, 0x00, 0x00, 0x00, 0x00, 0x00, 0x1F, 0xAA, 0x55, 0x00, 0x00, 0x70, 0x37};
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN WHILE */
HAL_UART_Transmit(&huart2, (uint8_t *)com_buff,sizeof(com_buff), HAL_MAX_DELAY);
HAL_UART_Transmit(&huart2, (uint8_t *)msg_screen,sizeof(msg_screen), HAL_MAX_DELAY);
while (1)
{
/* USER CODE END WHILE */
UartStatus = HAL_UART_Transmit(&huart1, (uint8_t *)tx_buff,sizeof(tx_buff), HAL_MAX_DELAY);
if (UartStatus != HAL_OK) {
HAL_Delay(10000);
}
HAL_Delay(10);
/* USER CODE BEGIN 3 */
}
I'm starting to have doubts on how uart transmit buffer works but i don't know where is my mistake
Thank you in advance
2021-06-18 5:03 AM
This issue was solved by changing some byte on buffer command.
Now i'm able to see my device responding using scope.
Using HAL_UART_Receive the read buffer is always empty and the function stuck on :
if (UART_WaitOnFlagUntilTimeout(huart, UART_FLAG_RXNE, RESET, tickstart, Timeout) != HAL_OK)
{
return HAL_TIMEOUT;
}
Does any one have an idea about that?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.