STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to access the 2KB user option bytes in H7

In the STM32H7 datasheets, page 23 (H750) or 26 (H743) - ST says the device has 2KB user option bytes flash area. Does anyone have idea if this is a typo? Or how to access this memory?If it really is there - it has a good potential to be used as conf...

Dan4 by Associate II
  • 7589 Views
  • 8 replies
  • 4 kudos

SPI loopbacking not working

I am using nucle-h745ziq ,SPI1 as Full duplex master and SPI4 as Full duplex salve.And both have same freuncy 25MHZ .And spi1 prescalar is 2.But SPI4 is not start the communication.Both structure parameter are same.In spi.c libabry I am uing if(HAL_...

MDeva.1 by Associate II
  • 3356 Views
  • 9 replies
  • 0 kudos

Is there a possibility of a mistake in stm32F4/7 reference manual About Encoder mode in Timer section?

We have three options to select encoder mode In SMS bits (Slave Mode Selection) of TIMx_SMCR register. Based on the description following each mode in this register, counter counts UP/Down on each TI2FP1/TI1FP2 edge based on the TI1FP2/TI2FP1 level o...

0693W00000BaLqKQAV.png 0693W00000BaLubQAF.png 0693W00000BaLuaQAF.png

How to excess DMA_SxNDTR register

I am trying to collect data from ADC using DMA in circular buffer mode.i want to excess/read DMA_SxNDTR register. also tell me how to read data from circular buffer. I have written code for reading count from DMA_SxNDTR but it is not working , it is...

0693W00000Bb9ZrQAJ.jpg
NKann.1 by Associate III
  • 1801 Views
  • 5 replies
  • 0 kudos

STM32G4 ADC1 DMA issue.

I am trying to read 3 ADC channels (ADC1) via DMA but I get false values in the watch window./* Private user code ---------------------------------------------------------*//* USER CODE BEGIN 0 */uint32_t value1[3];/* USER CODE END 0 *//** * @brief T...

PGand by Associate
  • 1122 Views
  • 1 replies
  • 0 kudos

Yet another "No ST-LINK detected! " issue

I have had STM32CubeIDE v1.3.0 working with my hardware. I just upgraded to Cube to v1.6.1. Now when I try to debug, I get "No ST-LINK detected! " message box This has happened before (my upgrade to 1.4.1 failed so I rolled back to 1.3.0). ST-LINK...

RWeil.3 by Associate II
  • 2340 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.