STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can any of the STM32H7 2 Kbytes (64 Flash words) of user option bytes be used for application configuration parameters

A similar question has been asked a few times on here. But I have yet to see a clear answer.In the document herehttps://www.st.com/content/ccc/resource/training/technical/product_training/group0/1f/4f/b7/85/91/e0/4d/2f/STM32H7-Memory-Flash_FLASH/file...

shami by Associate
  • 1456 Views
  • 1 replies
  • 1 kudos

How to capture NDTR of ADC DMA on timer event

Hi,on H723... I'm trying to configure a DMA on TIM5 CC3 event (DMA1 Stream 0 P2M) to capture the current NDTR value of another stream (DMA1 Stream 1 P2M) (to record where that DMA just put data from ADC into a ring buffer at the time of the CC3 event...

STM32F405RG 시리즈 문�?�

안녕하세요.기존�? 사용중�?� 시스템 (PIC 계열) �?서 MCU 만 �?체를 하여 사용�?� 하려고 합니다.기본 Digital I/O 신호가 5V �?��?�요.STM32F405RG �?� Datasheet 를 보면서 �?금�?�?� 있어 문�?�를 드립니다.​I/O structure 가 FT �?� 경우, 기존 사용하면 신호를 그대로 연결�?� 해�?� 무방한지요?아니면 Level shift 회로를 추가하는게 좋�?�지요?​​

CJeon.1 by Associate
  • 2961 Views
  • 1 replies
  • 0 kudos

STM32F207VCT6 COM Port Enumerates

Hi,I am Using STM32F207VCT6 on a project and after loading f/w image am seeing Windows COM Port enumerate on every new device it detects. VID / PID remain the same..Any ideas on this??

AKluk.1 by Associate II
  • 1953 Views
  • 3 replies
  • 0 kudos

Resolved! Transfer error on SAI4 DMA STM32H723ZE

Hi There,I'm looking for help with the SAI4 for this device. I have setup the DMA for SAI4A which is linked to BDMA Channel 2. I have defined my buffers within the D3 domain and have enabled the event on the BDMA channel to request number 15 (sai4_a...

KJans.1 by Associate II
  • 3684 Views
  • 5 replies
  • 0 kudos

Cannot program the MCU via the serial port USART1.

We are having a problem with programming the MCU via the serial port USART1. The pins used are TX: PA9 and RX: PA10.The serial port works as expected when we the application is running.BOOT0 ping seams to work. When low it boots our custom applicatio...

Resolved! IDE available for stm32

I wanted to know the IDE which are available for stm32.And whats the difference among them.

AR.7 by Associate II
  • 1514 Views
  • 2 replies
  • 0 kudos

Resolved! Core comunication using STM32H7

Hello, What is the best way to communicate between cores? I am working on a project in which I need to read data using one core and process this data using a second core. I am working with a STM32H745. The idea is that the M4 core is going to be used...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.