STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32N657xx Timer Clock(s)

I am confused about which clock(s) drive the timers.  In the reference manual is says the APB clock drives the timers but there are 5 APB clocks.  Also, in STM32CubeMX there is a "Timer Group Clocks".  What clocks drive which timers or is the one dri...

Resolved! Failure on GO Command of STM32G070

I have questions on the System Memory Boot Mode of the STM32G070CB MCUSetup:Access the System Memory Bootloader Mode every power cycle. Hence, I updated the Option Bytes as below:The MCU contains the Application image only; it does not contain a cust...

TesterSAM_0-1753438525495.png TesterSAM_0-1753438716884.png TesterSAM_1-1753438734226.png TesterSAM_2-1753438752242.png
TesterSAM by Associate III
  • 663 Views
  • 3 replies
  • 0 kudos

How to unbrick STM32C0

How to unbrick a C0 if user firmware reprograms SWD pins as IO? Because by default BOOT0 pin is disabled so there's no way to enter the bootloader unless it's enabled in OPTIONS bytes. I've added a failsafe 2 second delay at bootup before running any...

EP.2 by Associate III
  • 751 Views
  • 3 replies
  • 1 kudos

The F429 uses both SDRAM and SRAM

Whether the two buses can be used at the same time? Winbond's SDRAM is used to find a high probability of reading and writing errors in SDRAM data。 but there is no problem with using ISSI. If you don't read or write to the external SRAM, it's fine。

zyimi by Associate II
  • 361 Views
  • 1 replies
  • 0 kudos

Resolved! PDM microphone and filter options

I have compared my platforms using PDM microphones related to PDM to PCM and filtering:Platform 1:STM32H747 (Portenta H7), with SW PDM2PCM filter (and optional to add post-processing)Platform 2:STM32U5A5 with ADF filter (in MCU) or external PCMD3180 ...

PDM_MIC_comparison.png PDM_Filter_compare_animated.gif
tjaekel by Lead
  • 2970 Views
  • 2 replies
  • 0 kudos

Resolved! How to use STM32C071G8U6N correctly?

I bought few STM32C071G8U6N from Mouser few month ago.As I know, the SRAM size in spec is 24K, but I will get error message as below when ZI-data over 8KB"Error: L6406E: No space in execution regions with .ANY selector matching xxx.o(.bss)."Program S...

YST by Associate II
  • 1269 Views
  • 8 replies
  • 3 kudos

Measuring frequency - TIM2 value wrong

Hello, I have a project to measure the frequency (10Mhz) on an PA5 input and PWM output on PA6, with the counting triggered on PA0 (1PPS), CPU STM32F411, my problem is that the value TIM2 is always wrong, I must have around 10Mhz, I think that the co...

PSEBA.1 by Associate II
  • 2777 Views
  • 5 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.