STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H563ZI, Openocd configure and flash

Greetings! Getting back into embedded after a long while. As the title says I am wanting to use STM32H563ZI with openocd, but it is not supported out of the box. I have gone through the readme and it looks like I need to create a specific `target/stm...

tebel by Associate II
  • 7551 Views
  • 7 replies
  • 3 kudos

Resolved! STM32L073 operating on low power

Hi, I am working on a project where I have a custom board with STM32L073 MCU and I want to read a color sensor (AS7341) via I2C. This will be a low power application. I will harvest energy via NFC from a smartphone (I am using NTAG I2C plus). I can g...

sam111_0-1753287730279.png
sam111 by Associate II
  • 1665 Views
  • 9 replies
  • 3 kudos

Resolved! Unsolicited interrupts when temperature rises around 60°C

Hello,I am using a STM32L476RCT which should work up to 85°C.I am receiving unsolicited interrupts when I put my board in an environment at 60°C.I only use usart1 and a few GPIO interrupts, which are working fine. But when the temperature rises, the ...

gmaeng by Associate II
  • 1093 Views
  • 7 replies
  • 5 kudos

I did not get desired response while flashing GPIO demo

I am currently working on the STM32H7S78-DK board & after building GPIO demo present Example code from git repository of that STM32 provided, while flashing binary from the STM32 programmer I faced issue it is mentioned belowWhen code is flashed from...

amar_1_0-1753364633108.png
amar_1 by Associate
  • 431 Views
  • 1 replies
  • 0 kudos

STM32F413RGT6 uart HW bootloader V9.0

Hello, we use STM32F413RGT6 as slave board communicate through rs485 bus. In application, we drive rts by emulated gpio. We use for update of the board HW uart bootloader. Due to weakness of the HW bootloader we face some problems during update on ha...

krizp_0-1753712579042.png
krizp by Associate
  • 524 Views
  • 0 replies
  • 0 kudos

MCU with in-built GPIO input qualification

Hi all,I'm trying to find out if any STM32 MCUs support hardware input qualification on GPIOs, similar to what's available on TI C2000 MCUs.On the C2000 series, GPIOs can be configured for input qualification using a sampling window—typically 3 or 6 ...

ak52_0-1753689522481.png ak52_1-1753689568215.png
ak52 by Associate III
  • 685 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H563: No TRACECK present

Hi, I have configured my STM32H563AI CubeMX-project to use "JTAG with Trace  Synchro(4bits)" and assigned the corresponding pins. Also, I explicitly activated the corresponding registers in DBGMCU and DCB by adding: SET_BIT(DBGMCU->CR, DBGMCU_CR_TRA...

B1sh0p by Associate II
  • 1008 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.