2021-07-27 9:01 AM
Hi everyone
I'm trying to write the timer interrupt code I wrote in C (pa3 pin blinks at 10 ms intervals) with arm assembly language, but it doesn't work.I don't know exactly how to do the timer interrupt in assembly language.I tried to write my own code by looking at the disassembly feature from keil uvision. So where am I doing wrong? (I'm using stm32f103c8)
C code:
#include "stm32f10x.h"
void TIM2_IRQHandler()
{
TIM2->SR =0x00;
GPIOA->ODR ^=0x0008;//toggle pa3
}
int main(void)
{
RCC->APB2ENR = 0x04; /// port a
GPIOA->CRL = 0x00003000;
__disable_irq();
RCC->APB1ENR =0x1;// timer2
TIM2->ARR = 0xffff;
TIM2->PSC = 0x36; // 10hz
TIM2->DIER = 0x1;// (OVERFLOW)
TIM2->CR1 = 0x1; // TIMx_CR1.CEN
NVIC_EnableIRQ(TIM2_IRQn);
__enable_irq();
while(1)
{
}
}Assembly code
EXPORT Program
GPIOA_IDR EQU 0x40010808
GPIOA_CRL EQU 0x40010800
GPIOB_IDR EQU 0x40010C08
GPIOA_ODR EQU 0x4001080C
RCC_APB2ENR EQU 0x40021000
RCC_APB1ENR EQU 0x40021000
TIM2_ARR EQU 0x4000002C
TIM2_PSC EQU 0x40000028
TIM2_DIER EQU 0x4000000C
TIM2_CR1 EQU 0x40000000
TIM2_SR EQU 0x40000010
AREA start, CODE, READONLY
timer_ MOVS r0,#0x00
8372 MOV r1,#0x40000000
8376 STRH r0,[r1,#0x10]
8378 LDR r0,=GPIOA_ODR
8371 LDR r0,[r0,#0x00]
8372 EOR r0,r0,#0x08
8380 LDR r1,=GPIOA_ODR
8382 STR r0,[r1,#0x00]
ADDS R7,R7,#1 ;counter for debugging
8384 BX LR
Program MOVS r0,#0x04
8385 LDR r1,=RCC_APB2ENR
8390 STR r0,[r1,#0x18]
; pa3 out
MOV r0,#0x3000
LDR r1,=GPIOA_CRL
STR r0,[r1,#0x00]
ADDS R11,R11,#1
CPSID I
MOVS r0,#0x01
LDR r1,=RCC_APB1ENR
STR r0,[r1,#0x1C]
; TIM2->ARR = 0xffff;
MOVW r0,#0xFFFF
LSLS r1,r1,#18
STRH r0,[r1,#0x2C]
; TIM2->PSC = 54;
MOVS r0,#0x36
STRH r0,[r1,#0x28]
; TIM2->DIER = 0x1;
MOVS r0,#0x01
STRH r0,[r1,#0x0C]
; TIM2->CR1 = 0x1;
STRH r0,[r1,#0x00]
MOVS r0,#0x1C
BL timer_
CMP r0,#0x00
BLT interrupt ;
NOP
NOP
AND r2,r0,#0x1F
MOVS r1,#0x01
LSLS r1,r1,r2
LSRS r2,r0,#5
LSLS r2,r2,#2
ADD r2,r2,#0xE000E000
STR r1,[r2,#0x100]
ADDS R8,R8,#1 ;counter for debugging
NOP
interrupt NOP
ADDS R5,R5,#1 ;counter for debugging
MOVS R6,#0x3 ;control
CPSIE I
NOP
while B while
MOVS R6,#0x7
ALIGN
END
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.