2021-07-27 3:14 AM
2021-07-27 3:42 AM
Read the "Low power modes" subchapter of PWR chapter in RM.
You can simply use the __WFI(); intrinsic go to to sleep, any interrupt will wake up.
JW
2021-07-27 4:04 AM
thank you so much, but is it possible to use timers to wake the micro?
2021-07-27 4:46 AM
Of course!
Any interrupt can wake up from WFI. If you configure the timer to generate an interrupt, it will wake up the MCU.
2021-07-27 7:25 AM
Hello @Fghas.1,
You can refer to the examples provides by the STM32CubeF4 package.
As an example, the project under the "STM32Cube_FW_F4_V.XX\Projects\STM32F411E-Discovery\Examples\PWR\PWR_CurrentConsumption" path can help you configure the sleep mode and use the RTC configuration to set the timer to wake up from the low power mode.
Chahinez.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.