STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750 MPU XiP

Hey together,I have a question regarding MPU settings for an external QuadSPI Flash. We have a project where the full application code is placed onto the 4MB Quad SPI Flash memory W25Q32JVSIM. We have set up the QuadSPI in MemoryMapped moded and plac...

0693W00000D2Al3QAF.png
ESawa.1 by Senior
  • 3057 Views
  • 4 replies
  • 1 kudos

input capture

HiI launched a capture and sensitized the interrupt to both edges.I want to recognize each edge when intraoperating.I mean, to find out which edge was intraverted?I use micro stm32f407vgt

Hafsh.2 by Associate II
  • 3095 Views
  • 6 replies
  • 0 kudos

Resolved! STM32 Multi-threading/ multi functions

Hi,I am a newbie to STM controllers but I have worked on Arduino and Pi. I am thinking of working on STM because I have read that it supports multi threading, means we can perform multiple functions at the same time, as in high level languages. So, I...

OSmit.1 by Associate
  • 10131 Views
  • 1 replies
  • 0 kudos

cannot activate esim on P-L496-CELL02

I recently acquired a new P-L496G-CELL02 development kit to evaluate cellular communication performance. Out of the box, when I first plug in the P-L496G-CELL02 development kit to my PC and open a terminal, it instructs me to "open a web browser and ...

NKuma.9 by Associate II
  • 676 Views
  • 0 replies
  • 0 kudos

Problem with IWDG. does not reboot the MCU

I use STM32F042F6P6. I found that IWDG does not reboot the microcontroller. The program stops, but the microcontroller does not restart.At the time of IWG triggering, a short (at 0 then 1 again) is formed on the NRST pin, but the program is not resta...

EShai.2 by Associate II
  • 1672 Views
  • 4 replies
  • 0 kudos

Problem with HAL Timer Interrupt in KEIL MDK v5

Hello guys,i want to program a timer interrupt with HAL in the KEIL MDK v5 IDE. But i get a syntax error in the following line: HAL_TIM_Start_IT(&htim2); I get the following error message:error: expected parameter declaratorerror: expected ')'warnin...

TKlei.5 by Associate III
  • 1481 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.