2021-08-11 7:01 AM
Hi,
I am a newbie to STM controllers but I have worked on Arduino and Pi. I am thinking of working on STM because I have read that it supports multi threading, means we can perform multiple functions at the same time, as in high level languages. So, I want to know is it true?
Moreover, on which basic STM board should I work? As arduino UNO in Arduino platform. I have read that STM32 is most commonly used. So should I buy this one for learning?
Solved! Go to Solution.
2021-08-11 7:11 AM
Except for the more recent dual core MCUs, most STM32 are limited to running only one thing at a time, but you can use FreeRTOS or similar to have the system switch between tasks as needed, but this is not the same as multi-threading where multiple things are running simultaneously.
Any nucleo board is a cheap and good way to start learning. Let your project needs drive the decision on which to get. The one you linked is a knock-off board.
2021-08-11 7:11 AM
Except for the more recent dual core MCUs, most STM32 are limited to running only one thing at a time, but you can use FreeRTOS or similar to have the system switch between tasks as needed, but this is not the same as multi-threading where multiple things are running simultaneously.
Any nucleo board is a cheap and good way to start learning. Let your project needs drive the decision on which to get. The one you linked is a knock-off board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.