STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Bootloader information discrepancy

Reference Manual for STM32H72xxx/73xxx (RM0468), section 2.6, says that the embedded bootloader can be accessed via I2C1, I2C2, I2C3, I2C4 and SPI1, SPI2, SPI3, SPI4, however AN2606 only lists I2C1, I2C2, I2C3 and SPI, SPI3 as the working I2C and SPI...

HWidj.2 by Associate III
  • 1683 Views
  • 2 replies
  • 1 kudos

Error finishing flash operation

I have the following error when I was trying to debug using TrueStudio(v9.3.0).​The specific steps that caused the error are as follows.1. Connect STM32F100RB※1 to the PC.2. Launch TrueStudio(v9.3.0)3. make project 3.1 [File] -> [New] -> [C Projet] 3...

0693W00000D2PylQAF.png
Myasu.1 by Senior
  • 1362 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L052 USART: Problem Switchover from Output- to UART - TX - functionality produces a disturbing H/L - edge on TX

Two Usart - TX - lines shall be used either in PP- output- or in Usart - TX - mode.The switchover from a normal output pin to a Uart - TX - pin produces an High/ Low edge on TX followed by an interrupt on TX side.On RX- side this H/L edge causes an ...

FEber.1 by Associate III
  • 2301 Views
  • 4 replies
  • 0 kudos

FDCAN confusion

Hello,I hate to say this, but I am completely lost in regards to programming FDCAN to receive extended ID messages from an ECU. I looked to the examples provided in the IDE as well as other questions on this forum, but am still confused. I have a str...

Aaronium by Associate III
  • 1122 Views
  • 1 replies
  • 0 kudos

STM32F107 timers problem

Hi to all,I hope this is the right place where asking to.Anyway in my custom board I use four timers: SysTick, RTC, TIM6 (DAC) and TIM3 (PWM).I wnted to add a new timer (I tryed TIM7 and TIM2), but it wouldn't work and I discovered that neither TIM3 ...

STM32H725RG Maximum ADC Clock Rate in 16-bit Mode

I was reading this application note which lists maximum clock rates for the ADC on the STM32H7 for the various packages at different resolutionshttps://www.st.com/resource/en/application_note/dm00628458-getting-started-with-the-stm32h7-series-mcu-16b...

KYin.2 by Associate II
  • 1548 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.