STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Use LPTIM for the period measure.

I've clear (or at least I think so) how to use the timers (TIM), with "Input capture direct mode", in order to measure a period of one input pulse, but I don't understand how to do the same measure with the low power timer (LPTIM). The LPTIM associat...

FRest.1 by Associate III
  • 1478 Views
  • 2 replies
  • 0 kudos

Oscilloscope With External Trigger Using STM32F429 - Is it possible while taking the interrupt latency into account?

Hello,I'm planning to use the STM32F429 with its triple interleaved ADCs to make a 7.2Msps digital oscilloscope.So the thing about digital oscilloscopes is that they also record samples before the trigger events.To do so, they have a circular buffer ...

MMoha.3 by Associate III
  • 4687 Views
  • 8 replies
  • 1 kudos

How to configure SMT32F072x uC to access to NAND Flash memory?

I'm using a STM32F072x uC and would want to read/write/erase NADN flash (NAND04GW3B2B).A couple of questions:How to configure GOIP pins as an Input and Output Data Bus (D0 - D7 or I/O0 - I/O7) ?What are the exact sequences to read, write, erase, etc?...

Texram by Associate III
  • 1870 Views
  • 3 replies
  • 0 kudos

How to read data correctly from NEO-6M GPS module?

Hi.I am trying to read data from the GPS module using USART1 and then send to to a serial monitor through USART2. It ended up not printing the information correctly on the serial monitor. (I have tried to connect the GPS module to a FTDI module direc...

0693W00000D1pAQQAZ.png
M7890.1 by Associate III
  • 7064 Views
  • 12 replies
  • 0 kudos

I cannot obtain any design resources regarding PFC/DPS, st-pld, st-wds, which neither provides open source code nor can I visit www.biricha.com.

I am designing PFC & DPS using STM32G474, I also bought a NUCLEO discovery kit, but I cannot obtain any design resources regarding PFC/DPS, st-pld, st-wds, which neither provides open source code nor can I visit www.biricha.com. And I believe www.bir...

HXU.1 by Associate
  • 1786 Views
  • 3 replies
  • 0 kudos

Resolved! Logins Broken By New Password Rules

There doesn't seem to be anywhere to post issues with the forum itself?I couldn't login this morning - the site kept saying my password was wrong.I know that it wasn't wrong, because I copy it from a password manager.So I had to do a password reset.T...

SWD Data Trace timestamp 0

Hi there,when I try to log my ADC data with the SWD Data Trace I can see every write access to my variable but the timestamp becomes 0 after the fourth sample. Attached is a screan shot to show what I mean. After quite a while the <cycles> tap switch...

0693W00000D2XUAQA3.png
LGard.1 by Associate II
  • 839 Views
  • 0 replies
  • 0 kudos

I2C commands to LCD

I am learning this new 32-bit from my 8-bit world as well as new IDE on top of re-learning C. So be gentle....I am trying to use the CubeIDE to talk to an I2C LCD. I am following a tutorial but the LCD does not respond at all.Some of the code below...

SScot.3 by Associate II
  • 11814 Views
  • 17 replies
  • 0 kudos

Resolved! STM32 UART on android

How to connect to UART via USB on android device? Do I need some driver on android device?​Stm32L432KC nucleo​

oeliks by Senior
  • 2490 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.