2021-08-15 2:46 AM
Reference Manual for STM32H72xxx/73xxx (RM0468), section 2.6, says that the embedded bootloader can be accessed via I2C1, I2C2, I2C3, I2C4 and SPI1, SPI2, SPI3, SPI4, however AN2606 only lists I2C1, I2C2, I2C3 and SPI, SPI3 as the working I2C and SPI interfaces used.
I didn't notice any discrepancy with the other interfaces.
Can someone help to clarify?
Solved! Go to Solution.
2021-08-17 5:04 AM
Hello @HWidj.2 ,
AN2606 is correct.
For STM32H72xx/3xx, the bootloader have I2C1/I2C2/I2C3 and SPI1/SPI3/SPI4 (no SPI2).
Thank you for noticing that. The RM0468 will be fixed in the coming releases.
When your question is answered, please close this topic by choosing Select as Best. This will help other members of the community find this response more quickly. :)
Imen
2021-08-17 5:04 AM
Hello @HWidj.2 ,
AN2606 is correct.
For STM32H72xx/3xx, the bootloader have I2C1/I2C2/I2C3 and SPI1/SPI3/SPI4 (no SPI2).
Thank you for noticing that. The RM0468 will be fixed in the coming releases.
When your question is answered, please close this topic by choosing Select as Best. This will help other members of the community find this response more quickly. :)
Imen
2021-08-17 8:42 AM
Thanks for the clarification.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.