STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L072 slow start-up time

I'm using a STM32L072CZT6 in a mobile application in which I need the MCU to start up as fast as it can. Currently the start-up time is 6ms. That appears to be too long based on this thread (Start-up time too long), although I haven't found a typical...

MBles.1 by Associate II
  • 7624 Views
  • 8 replies
  • 0 kudos

Resolved! Why does configuration tool code generator changes my code in main between /* USER CODE BEGIN 5 */ and /* USER CODE END 5 */? I thought user code sections where untouched? What can be wrong?

Everytime i run code generator, the main file is changed between User Code ? */ /* USER CODE END Header_StartDefaultTask */ void StartDefaultTask(void const * argument) { /* USER CODE BEGIN 5 */ /* Infinite loop */ for(;;) { LedTask(); ...

sde c.1 by Senior II
  • 1020 Views
  • 3 replies
  • 0 kudos

Resolved! Hi, good morning, I have a compilation error what I add Flash functions such as HAL_FLASH_Unloc() ... I don't understand why, maybe I miss a setting in the project. The microcontroller is ESP32G070xx. Can anyone help me? Thank you very much Julian

#include "stm32g0xx_hal.h"  HAL_FLASH_Unlock();  FLASH_Erase_Sector( FLASH_SECTOR_11,VOLTAGE_RANGE_1 );  HAL_FLASH_Lock();ERROR:../Drivers/CMSIS/Device/ST/STM32G0xx/Include/stm32g070xx.h:531:31: error: expected declaration specifiers or '...' before ...

JMigl.1 by Associate
  • 2192 Views
  • 3 replies
  • 0 kudos

Resolved! Is 0 lowest or highest priority?

Hi, its not clear for me, does lower number represent higher or lower priority?Is "System tick timer" at highest or lowest priority?

0693W00000Dq4JXQAZ.jpg
JBond.1 by Senior II
  • 2091 Views
  • 1 replies
  • 0 kudos

rms value measurement in stm32f030c6t6

dear experts i am working on stm32f030c6t6 MCU i want to calculate the adc measurement of sine wave form at Gpio pin and that gpio pin has a adc channel also i am using the DMA here i am using another Adc channel for other purpose please check my cod...

Sbomm.1 by Associate
  • 2278 Views
  • 2 replies
  • 1 kudos

Resolved! USART 2 Transmit not working

Board : STM32F746GI configure USART1 with same configuration. USART1 is working fine. I did same configuration for USART2 also, but USART2 not working. I don't know what's happening.Thanks Manikandan D

Mani1 by Associate II
  • 5628 Views
  • 9 replies
  • 0 kudos

Push button: is there a need for software debouncing?

Hi. I am trying to trigger and external interrupt using a push button (rising edge trigger and use internal pull down). When the push button is pushed, the variable cnt should be incremented and the pulse width of the PWM shall be changed according;...

M7890.1 by Associate III
  • 5366 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.