STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Loading the 2 applications from Flash memory

I am working on STM32L151RCT6 controller in STMcube IDE.. i have one application running in the Flash from starting address and one more application i want to run it from other location of Flash..basically 2 block of firmware(applications) i am consi...

MBhir.11 by Associate III
  • 1709 Views
  • 1 replies
  • 1 kudos

STM32H743 Internal Flash (single sector) going bad

Hi,I had a question with respect to the internal flash of the stm32 chip that we are using. After much investigation, it seems that the erase operation (via the HAL_FLASHEx_Erase_IT() function in software or using the ST-link utility directly) is "sl...

PSari.1 by Associate II
  • 5232 Views
  • 11 replies
  • 0 kudos

Run two DMAs simultaneously on STM32F407

I am working on a project that uses an STM32F4 disc board to read and write external ADC and DAC with two SPI interfaces. SPI1 (DMA2 Stream3) is set to TX only to write waveform to a DAC, and SPI3 (DMA1 Stream0) is set to RX only to read an ADC. Whe...

PLi.4 by Associate II
  • 3910 Views
  • 8 replies
  • 0 kudos

Hi everyone, I'm a beginner with MCUs. I want to read ADC values from 12 channels continuously and I'd like to implement an averaging process before transmitting them through UART. I'm using Nucleo-L476RG.

Signals are similar across all 12 channels but I'm confused about how to run the averaging algorithm for 12 channels at the same time. Currently, I can get the ADC values from all 12 channels using DMA without the averaging process.To explain further...

AMahm.1 by Associate II
  • 3835 Views
  • 7 replies
  • 0 kudos

STM32H745ZI(LQFP144) FMC and SDRAM support

Hello ST community! I have a question about FMC on STM32H745ZITx (LQFP144). In the datasheet DS12923 (https://www.st.com/resource/en/datasheet/stm32h745zg.pdf) it is not said whether it supports SDRAM. And there is no "SDRAM" item in the FMC settings...

0693W00000Dq8MzQAJ.png 0693W00000Dq8MpQAJ.png
AAlek.2 by Associate II
  • 3039 Views
  • 5 replies
  • 1 kudos

mdma linked list unconditionnal trigger to next block

Hello,I am learning MDMA, and have been able to make it work in different scenarios, but I am now stuck.I want to use MDMA to chain DMA transactions without CPU intervention.What I want to do with mdma linked list is :° configure timer in output° use...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.