STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Incorrect RTC operation in STM32L073CZ

Good afternoon.I have developed a device for collecting data from sensers and storing them in external memory.During testing, I revealed a failure in the operation of the device.Investigation of the behavior showed that there is an error in the RTC o...

AManu.1 by Associate II
  • 2674 Views
  • 6 replies
  • 0 kudos

MCU boot

I designed Control card using stm32f205vet6 and it working good. But when I changed MCU  to stm32f205vbt6 I have boot problem. boot address is  0x1fff3de4 so MCU is not working.

sözme.1 by Associate
  • 1033 Views
  • 1 replies
  • 0 kudos

High jitter on MCO output?

I just got my NUCLEO-H723ZG board, I loaded the GPIO_InfiniteLedToggling example project, downloaded the program to the board and it worked fine. Then I added a very simple code to output the HSE clock to an MCO pin. /* Enable the MCO1 Clock */ LL_...

HWidj.2 by Associate III
  • 5288 Views
  • 10 replies
  • 0 kudos

Extended CAN2.0B filtering in List mode problem

Hello, In my system I have extended canbus with 29b identifier. With mask filtering it looks to be working, but list filtering gives me problems; ( i have setup where on STM32 is sending data with with any ID I want, and second is capturing data as w...

Linas L by Senior II
  • 1008 Views
  • 0 replies
  • 0 kudos

How to active WS2812LED on stm32G071CB?

Hi,I took code from:https://controllerstech.com/interface-ws2812-with-stm32 and made the adjustment to my MCU (stm32G071CB). but it didn't work.I manage to generate pulses from PWM with DC of 66% in 800K but not through DMA. I also try to ran it fro...

SAram.11 by Associate
  • 1714 Views
  • 2 replies
  • 0 kudos

Interrupt not working after jump to code from bootloader

I have a project that consists of a bootloader and 2 pieces of code on STM32L100R8. The bootloader correctly switches to the relevant piece of code but it seems as though when the code receives it first interrupt it fails. Attached are screenshots of...

0690X000006C8etQAC.jpg 0690X000006C8eoQAC.jpg 0690X000006C8ejQAC.jpg
spack by Associate
  • 6235 Views
  • 9 replies
  • 0 kudos

Resolved! Timer Compare output enable on multiple pins

Hi All,I'm playing around with the Timers at the moment on a STM32F303 and currently have TIM2 and TIM6 generating an output pulse on every OC event (different frequency ranges).Those Timer based output toggles are of course somewhat locked to certai...

RMyer.1 by Associate III
  • 1888 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.