STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 STLINK Detect problem

HelloI am using stm32f072c8t6 in my project but stlink does not connect stm32 somehowHow can I detect the fault?boot pin > 10k > GNDNRST pin>10k 3.3v

0693W00000DlwLNQAZ.jpg
Operi.1 by Associate II
  • 2139 Views
  • 4 replies
  • 0 kudos

ST Visual Programmer Warnig(The device is protected)

When I tried to write a file to STM32F103RCT6, it could not be written.STVP displays this as a "device protected" warning.The IC was purchased from a trading company and is not written to the cash register.We inspected nearly 70, but not the other bo...

YBAN.1 by Associate
  • 1574 Views
  • 2 replies
  • 0 kudos

I am trying to find any information about what the values I would read using Differential inputs from ADC's on STM32F303. IS there Documents about Differential input (what the output would be)?

I am using STM32F303REx to measure Voltage and Current from ADC (differential Input). Is there -+ values around 0 or are they offset around 4096/2 Offset that must be subtracted to get a signed value? Is there any documentation or Examples?

DWise.1 by Associate II
  • 1531 Views
  • 2 replies
  • 0 kudos

Nucleo-L412 Programming Error

Hi. I have Nucleo-L412 programming error with Keil. I can program Nucleo F401, F411 and F407 discovery board without error. But I can not load the program to the L412 board. I had had "No ST Link Detected error" but then I solved this problem on Keil...

MÇeli.2 by Associate II
  • 1139 Views
  • 1 replies
  • 0 kudos

Problem with RTC on STM32G0.... family MCU

HI,good mornig,I'm starting to use RTC on STM32G0...familyI'm using NUCLEO board G071RB for initial tests and I setted it as follow:1) introducing 2032 battery on Vbat pin (previous disconnect SB26 jumper (Vdd))2) select LSE by STCubeMX configuration...

FSpre.1 by Associate
  • 2255 Views
  • 2 replies
  • 0 kudos

Stm32f030c8t6 clock problem

Hi everyone i have stm32f030c8t6 mcu with out evaluate borad, when i set the clock on 8 Mhz it's work correctly, but when i set the clock on 16,32Mhz with pll or even with HSE it doesn't work, i check in keil debug and it writes cannot access memory,...

MSafa.3 by Associate
  • 1989 Views
  • 3 replies
  • 0 kudos

Resolved! Are there any tools available for debugging memory leaks?

I'm using an STM32F767ZI, and am programming it in C without any additional libraries (bare metal).I believe there is a memory leak somewhere as a memory allocation that typically would work seems to fail after the program has been running for some t...

Starman by Associate II
  • 6359 Views
  • 10 replies
  • 0 kudos

Where Can I Find Latest Libraries?

In the past, I'd pull them from CUbe, but the ones I have seem out of date. Is there somewhere else I can get the standard peripheral libraries (on the website maybe)?

jvavra by Associate III
  • 1141 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.