2021-09-01 12:36 PM
Hi. I have Nucleo-L412 programming error with Keil. I can program Nucleo F401, F411 and F407 discovery board without error. But I can not load the program to the L412 board. I had had "No ST Link Detected error" but then I solved this problem on Keil "Debug-(Add) Flash Download" preferences. Now it looks like I can download the code to the Nucleo but It does not work even Blinky program. JP1 pin is On.
2021-09-01 12:48 PM
Next logical step would be to debug the code, step through, see if it's stopping somewhere or if it's trying to run the LED code.
JP1 ON holds the ST-Link in reset. How are you able to download code like this? Are you using an external programmer?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.