STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f412 i need much more clock speed!!

hello every one. im running something that needs high clock speed. actually i want to create picture with some moving LEDs. i have 75MHz on gpio but its not enough. i just know its possible. im using register codes. im using boolean array for image d...

Mesl.1 by Associate
  • 1319 Views
  • 2 replies
  • 0 kudos

STM32L0+: The RTC-Wake-Up_timer with __WFE()-sleep-entry delivers two wake ups instead of one wake up. And this consumes more power then needed.

__WFI():  (Wake up by Interrupt):leads to a one wake up as expected but swallows some interrupts if more interrupt sources are simultaneously produce interrupts. The understanding of this behavior costed me a lot of time.       __WFE():  (Wake up by ...

FEber.1 by Associate III
  • 893 Views
  • 0 replies
  • 0 kudos

Resolved! Can I use disabling of certain low-power timer (LPTIMx) by clearing the ENABLE bit in the LPTIM_CRx register safely if no interrupts from LPTIMx are used to wake up MCU from Stop mode?

Clarification: Can I be sure that the case in Errata sheet ES0491 "Device may remain stuck in LPTIM interrupt when entering Stop mode" never occurs for certain LPTIMx if no interrupts within it are used to wake up MCU from Stop mode and disabling of ...

STM32G4 flash write/erase

I'm quite confused. The RM0440 states: "Note that read-while-write capability (or RWW) is only supported when the dual-bank architecture is active. This enables programming or erasing one bank while executing code from the other bank." Okay, for me, ...

BMcK by Associate III
  • 10196 Views
  • 16 replies
  • 0 kudos

stm32L452 HAL_SD_WriteBlocks_DMA without irq response

It is the problem about the dma driver of stm32L452's sdmmc1.ide: cubeideboard: NUCLEO-L452REconfig: sdmmc1 with dma , sd 4bit, without rtossdmmc1 dma config : 1. {sdmmc1 both(rx and tx) : dma2_channel_4} or 2. {(sdmmc1_rx : dma2_channel_4) and (s...

Cchn.1 by Associate II
  • 839 Views
  • 0 replies
  • 0 kudos

Debug infrastructure in STM32F7

For a long time I have been trying to guess how debug components are connected to the Cortex-M7 core in STM32F7 series of microcontrollers. It is supposed to be shown in e.g. the document RM0410 in Figure 587. This figure seems to be a copy of the sa...

MirKoz by Associate III
  • 1716 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.