2021-09-02 1:52 AM
I am currently experimenting with programming flash memory. I want to figure out how many sectors to erase before writing data into memory. I came across the following snippet
uint32_t Flash_Write_Data (uint32_t StartSectorAddress, uint32_t *Data, uint16_t numberofwords)
{
static FLASH_EraseInitTypeDef EraseInitStruct;
uint32_t SECTORError;
int sofar=0;
/* Unlock the Flash to enable the flash control register access *************/
HAL_FLASH_Unlock();
/* Erase the user Flash area */
/* Get the number of sector to erase from 1st sector */
uint32_t StartSector = GetSector(StartSectorAddress);
uint32_t EndSectorAddress = StartSectorAddress + numberofwords*4;
uint32_t EndSector = GetSector(EndSectorAddress);
/* Fill EraseInit structure*/
EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
EraseInitStruct.VoltageRange = FLASH_VOLTAGE_RANGE_3;
EraseInitStruct.Sector = StartSector;
EraseInitStruct.NbSectors = (EndSector - StartSector) + 1;
/* Note: If an erase operation in Flash memory also concerns data in the data or instruction cache,
you have to make sure that these data are rewritten before they are accessed during code
execution. If this cannot be done safely, it is recommended to flush the caches by setting the
DCRST and ICRST bits in the FLASH_CR register. */
if (HAL_FLASHEx_Erase(&EraseInitStruct, &SECTORError) != HAL_OK)
{
return HAL_FLASH_GetError ();
}
/* Program the user Flash area word by word
(area defined by FLASH_USER_START_ADDR and FLASH_USER_END_ADDR) ***********/
while (sofar<numberofwords)
{
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, StartSectorAddress, Data[sofar]) == HAL_OK)
{
StartSectorAddress += 4; // use StartPageAddress += 2 for half word and 8 for double word
sofar++;
}
else
{
/* Error occurred while writing data in Flash memory*/
return HAL_FLASH_GetError ();
}
}
/* Lock the Flash to disable the flash control register access (recommended
to protect the FLASH memory against possible unwanted operation) *********/
HAL_FLASH_Lock();
return 0;
}Here end sector calculation is done by adding the product of numberofwords and 4 to start address. Can some one explain the intuition behind this ?
Solved! Go to Solution.
2021-09-02 1:57 AM
On the STM32, the length of a word is 32 bits, which is 4 bytes.
2021-09-02 1:57 AM
On the STM32, the length of a word is 32 bits, which is 4 bytes.
2021-09-02 2:31 AM
so each address holds a byte of data correct?
2021-09-02 2:37 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.