STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI2 Communication on STM32H743X

I have been using STM32H743x for a project. There i use SPI2 to communicate with a serial flash IC.I need different packet sizes when accessing the Flash. The problem i have is, when i change the TSIZE at different stages, the firmware freezes at the...

SFons.1 by Associate II
  • 1795 Views
  • 2 replies
  • 0 kudos

Resolved! USB virtual com port can't receive data when device reboot

Hello,​I experienced a phenomenon in which the USB port was not reconnected.This phenomenon occurs when a USB port is connected to the product and reboots.​I check my device manager. When i turn off product, com port also disappear.and product reboot...

0693W00000Dmc7wQAB.png
hjuns by Associate III
  • 2281 Views
  • 4 replies
  • 0 kudos

Do not erase a sector on subsequent SW uploads

Hello, I'm using a STM32F103 and my code needs to save a few parameters from calibration activities in factory in the FLASH. I have successfully configured the last sector and I use it.Then, what I'd like is:FLASH the STM32 with the whole SW the 1st ...

LaoMa by Associate III
  • 3149 Views
  • 5 replies
  • 1 kudos

Resolved! Question regarding FFTs in arm_math.h

Hello! I am trying to simulate an octave model on a microcontroller and ran into a snag I thought I'd get some help with. So I have an FFT I am running on a sample of data (we'll say 4096 bytes). In octave, I'm using an FFT of the sample (where the s...

JayDev by Senior II
  • 6622 Views
  • 8 replies
  • 0 kudos

Boot0 pin on STM32L011 has internal pull resistor?

Hello all.I'm using BOOT0-PB9 pin on a STM32L011. In the reference manual I've found that "The pin logic level can then be read as an input value on the shared GPIO pin.", but nothing about internal pull resistor.The question is: is this pin provided...

hi iam trying to find FFT using stm32F4 discovery board. i have tried using CFFT and RFFT available in arm CMSIS DSP library but iam getting wrong answers. Can someone please tell me where iam wrong. Iam posting the code below for both RFFT and CFFT ?

-----------------------------------------------------------------*/ #include "main.h" #include "usb_host.h"   /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #define ARM_MATH_CM4   #incl...

Vk.2 by Associate II
  • 1242 Views
  • 0 replies
  • 0 kudos

Resolved! UART RECEIVE PROBLEM / STM32G061C6

Hi all,I am using a STM32G061C6T6 MCU. I'm trying to contact Nextion HMI. My data sending is successful, but I can't get any data. I couldn't run any of the Pooling and interrupt methods when receiving data. When I follow the RX pin with the oscillos...

0693W00000DmdEtQAJ.png

Communication via RS485 stop working after random time

Hi everybody,This is the first time I'm writing in a forum so I'm sorry if I didn't right.I'm developed a board based on STM32F091VBT.I'm using this board to communicate with other devices (two touch, a gateway and another board based on STM32F091VBT...

JDame.1 by Associate
  • 3213 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.