2021-09-09 4:25 AM
-----------------------------------------------------------------*/
#include "main.h"
#include "usb_host.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#define ARM_MATH_CM4
#include<stdbool.h>
#include<math.h>
#include"arm_math.h"
#include"arm_common_tables.h"
#include"arm_const_structs.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
#define SAMPLES 128 /* 256 real party and 256 imaginary parts */
#define FFT_SIZE SAMPLES / 2 /* FFT size is always the same size as we have samples, so 256 in our case */
#define SAMPLING_RATE 5000
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;
I2S_HandleTypeDef hi2s3;
SPI_HandleTypeDef hspi1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
uint8_t data[10];
uint8_t data2[10];
uint8_t data1[]="\r\n";
uint8_t data3[]="\t";
//float real_fsample = 10000;//sampling frequency
int k=0;
float t;
float32_t Input[SAMPLES];
float32_t Output[FFT_SIZE];
float32_t frequencybin[FFT_SIZE];
float32_t maxValue,peakfrequency,ratio; /* Max FFT value is stored here */
uint32_t maxIndex; /* Index in Output array where max value is */
uint8_t outarray[14];
char charArray[10],charArray1[10];
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_I2S3_Init(void);
static void MX_SPI1_Init(void);
static void MX_USART2_UART_Init(void);
void MX_USB_HOST_Process(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
arm_cfft_radix4_instance_f32 S; /* ARM CFFT module */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
MX_I2S3_Init();
MX_SPI1_Init();
MX_USB_HOST_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
HAL_UART_Init(&huart2);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();
/* USER CODE BEGIN 3 */
for ( k = 0; k< SAMPLES; k+= 2) {
t=k*.0002;
/* We assume that sampling and other stuff will take about 1us */
/* Real part, must be between -1 and 1 */
Input[(uint16_t)k] = (float32_t)((float32_t).7*sin(2*3.14159*120*t));
/* Imaginary part */
Input[(uint16_t)(k + 1)] =0.0;
}
arm_cfft_radix4_init_f32(&S, FFT_SIZE, 0, 1);
/* Process the data through the CFFT/CIFFT module */
arm_cfft_radix4_f32(&S, Input);
/* Process the data through the Complex Magniture Module for calculating the magnitude at each bin */
arm_cmplx_mag_f32(Input, Output, FFT_SIZE);
/* Calculates maxValue and returns corresponding value */
arm_max_f32(Output, FFT_SIZE, &maxValue, &maxIndex);
ratio=(float)SAMPLING_RATE/SAMPLES;
peakfrequency=ratio*maxIndex;
}/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "usb_host.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#define ARM_MATH_CM4
#include<stdbool.h>
#include<math.h>
#include"arm_math.h"
#include"arm_common_tables.h"
#include"arm_const_structs.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
#define SAMPLES 128 /* 256 real party and 256 imaginary parts */
#define FFT_SIZE SAMPLES / 2 /* FFT size is always the same size as we have samples, so 256 in our case */
#define SAMPLING_RATE 5000
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
uint8_t data[10];
uint8_t data2[10];
uint8_t data1[]="\r\n";
uint8_t data3[]="\t";/* USER CODE BEGIN PM */
float real_fsample = SAMPLING_RATE;
float32_t Input[SAMPLES];
float32_t Output[SAMPLES],t,output[FFT_SIZE];
float32_t maxValue,peakfrequency;
float32_t frequencybin[FFT_SIZE],ratio;
uint32_t maxIndex;
char charArray[10],charArray1[10];
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;
I2S_HandleTypeDef hi2s3;
SPI_HandleTypeDef hspi1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_I2S3_Init(void);
static void MX_SPI1_Init(void);
static void MX_USART2_UART_Init(void);
void MX_USB_HOST_Process(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
MX_I2S3_Init();
MX_SPI1_Init();
MX_USB_HOST_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
HAL_UART_Init(&huart2);
arm_rfft_fast_instance_f32 fft_handler;
arm_rfft_fast_init_f32(&fft_handler, SAMPLES);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();
/* USER CODE BEGIN 3 */
for(int i=0;i<SAMPLES;i++)
{
t=i*.001;
Input[i]=.7*sin(2*3.14159*50*t);
}
ratio=(float)SAMPLING_RATE/SAMPLES;
for(int i=0;i<FFT_SIZE;i++)
{
frequencybin[i]=ratio*i;;
}
arm_rfft_fast_f32(&fft_handler,Input,Output,0);
arm_cmplx_mag_f32(Output,output, SAMPLES);
arm_max_f32(output, FFT_SIZE, &maxValue, &maxIndex);
ratio=(float)SAMPLING_RATE/SAMPLES;
peakfrequency=ratio*maxIndex;
for(int i=0;i<FFT_SIZE;i++)
{
frequencybin[i]=ratio*i;;
}
/* USER CODE END 3 */
}Iam also confused regarding sampling frequency. where i sit given in the fft library?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.