STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC(with DMA) doesn't work when I increase its frequency

This has been a reoccurring issue for me, whenever I raise the ADC frequency above 0.25MHZ the while loop gets interrupted, and when I use frequencies below that the ADC resolution drops to 8 bits for an unknown reason. Is there a way to fix this wi...

0693W00000FAuNaQAL.png 0693W00000FAuHxQAL.png 0693W00000FAuMXQA1.png 0693W00000FAuMDQA1.png
HAbay.1 by Associate III
  • 3451 Views
  • 8 replies
  • 1 kudos

Contents of the unique device ID registers LOT_NUM

I'm using STM32L031E6Y6 for a high volume low cost product and I'm hoping to arrange it so that even if my firmware binary were to be stolen, it could only be used to produce a limited number of counterfeit products.I can cryptographically fix the fi...

MMora.6 by Associate II
  • 1359 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G0B1KBU7 (UFQFPN32) and clock for FDCAN peripheral

Hello,We are planning on replacing the F042 (TSSOP20) with the G0 cited in the question.At the moment the F042 use a HSE crystal of 8MHz in order to get a precise enough clock for the CAN peripheral.Parsing the datasheet of the G0B1KB, there is no wa...

Kraal by Lead
  • 2196 Views
  • 5 replies
  • 0 kudos

Experience with oddly silkscreen STM32s?

Got a new batch of micro's from a broker due to the chip crisis. They work and soldered down fine, memory matched, bootloader, etc. The concern about these MPU's is the silk screen and die marks are quite different.We have never seen die marks on the...

0693W00000FAjE8QAL.png
RCyr.1 by Associate
  • 2390 Views
  • 4 replies
  • 0 kudos

STM32H743ZI UART Tx with DMA doesn't want to turn on

Hi guys, its been a while and I hope everyone is well and safe.Using a STM32H743ZIReference Manuel I am having issues turning on the DMA1 stream associated to the UART4 Tx, in this case DMA1_Stream1. The DMA is setup as a One Shot mode (Normal Mode) ...

CLeo.1 by Senior II
  • 2174 Views
  • 5 replies
  • 0 kudos

STM32f746G_DISCO board sdram configuration quesiton

Hi, In the STM32F746G_DISCO board, FMC_SDRAM example, how to decide these parameters? Which section does it specify from sdram MT48LC4M32B2B5 datasheet? SDRAM_Timing.LoadToActiveDelay   = 2; SDRAM_Timing.ExitSelfRefreshDelay = 6; SDRAM_Timing.SelfRe...

JChen.24 by Associate III
  • 1088 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.