STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H743 RTC Wakeup

Im trying to configure RTC for periodic autowakeup, and have no clue why it is now working properly. RTC_WKUP_IRQHandler called immediately and again and again, even though wakeup flag is cleared, resulting 2.4 MHz at LED2 (LED2_GPIO_Port->ODR ^= LED...

Resolved! STM32G0: Remapping address 0x00000000 to SRAM does not work

Hello,I'm using a STM32G0B1CC and I'm trying to remap address 0x00000000 to SRAM like this: __HAL_RCC_SYSCFG_CLK_ENABLE(); __HAL_SYSCFG_REMAPMEMORY_SRAM();Unfortunately this does not work and 0x00000000 is still mapped to FLASH.If I try to remap t...

DaMCU by Associate II
  • 4122 Views
  • 7 replies
  • 1 kudos

Resolved! How to generate PWM and use timer interrupt at the same time?

I am using the Bluepill board. I want to generate PWM signal on Timer2 and set up a timer interrupt at 20ms interval on Timer3. I realized that the PWM signal cannot be generated if I set up the timer interrupt on Timer3. How do I solve this problem?

M7890.1 by Associate III
  • 21822 Views
  • 11 replies
  • 0 kudos

How to prevent uploading a new sketch to a Nucleo board

 I hope this thread is posted in the right category.I’ve been using Arduino boards for several years and am thinking of using a Nucleo 144 board (specifically, Nucleo-F207ZG) for a project. Once the project is completed, it will be serve as a permane...

Saint32 by Associate II
  • 4134 Views
  • 8 replies
  • 0 kudos

Determining RAM size at Runtime?

There's the Flash Size Register in the Device electronic signature. Is there an equivalent for the onboard SRAM size? Any way to get the ACTUAL SRAM size at runtime?

LMore.5 by Associate II
  • 2432 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.