STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to set up the adc sampling time.

Hi,I am using ADC of STM32H743ZI which is configured as 16 bit, ADC clock =36.5MHz,Tsampling=1.5cycles in continuous conversion mode . I am using DMA technique to collect the data using a buffer size of 4096 in circular mode.The input is sine wave o...

GHARI.1 by Associate II
  • 20454 Views
  • 18 replies
  • 0 kudos

UART information is shifted by 1 byte when I connect my STM32G474RE directly to my PC and use a terminal program to send information to control things. It fixes itself after resetting the board.

For example, if I send 1000, it will be received as 0100 on the STM board. I send what I received in the Rxcallback function. My program doesn't work, so I know this is the case. This issue stops after I hit the RESET switch on my board. Now, my iss...

Resolved! Availability of FDCAN peripheral on port C pins of STM32G0B1RE

Hi,Parsing the datasheet DS13560 of the STM32G0B1RE device, there is a discrepency between table 12, where some pins of port C have the FDCAN peripheral listed as alternate function, however it is not present in table 13.On the contrary, PE0 and PE1 ...

Kraal by Lead
  • 1193 Views
  • 1 replies
  • 0 kudos

ssd1327 oled display interfacing with stm32

Hi have been working on the interfacing of ssd1327 with stm32 microcontroller, i am just trying to print a pixel on the display but I could not display it. my code is as follows WRITECOMMAND(0xae); // WRITECOMMAND(0x15); WRITECOMMAND(0x00); WRITECOMM...

NJP.1 by Associate III
  • 2026 Views
  • 1 replies
  • 0 kudos

Utilizing discover board STM32F407 with FPU

Hello! I am utilizing discover board STM32F407 with FPU , The board is ARM cortex M-4 based. I want to use FPU to quick the process of conducting exponent calculations and Floating point. I have set down all peripheral drivers that are required for a...

by Not applicable
  • 1689 Views
  • 2 replies
  • 0 kudos

Resolved! unexpected waveform in Examples/OPAMP/OPAMP_PGA/ in G4 package

I try to learn how to use OPAMP by testing the example code Examples/OPAMP/OPAMP_PGA/.The MCU board is Nucleo-G431RB.This is the case of OPAMP_PGA_GAIN_2_OR_MINUS_1: blue line is output by DAC and red is by OPAMP. My 1st question: why the amplified s...

0693W00000DntA6QAJ.jpg 0693W00000DntCRQAZ.jpg
HDaji.1 by Senior
  • 5452 Views
  • 12 replies
  • 0 kudos

Resolved! Can you help me verify the schematic of STM32L476RGT6U?

I'm mounting my MCU on PCB. I have done the schematic referring from https://www.st.com/resource/en/datasheet/stm32l476je.pdf . Please help me verify this. My conditions are as follows.I am using 2 Digital sensors and one LoRa as communication module...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.