STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H725 ADC3 DMA

I read the adc value using ADC3 + DMA using STM32H725.​ADC3 channel 0,1,10,11 are reading adc value. ​1) ADC3 + DMA1 : RAM 0x24000000 ~ 0x2401FFFF2) ADC3 + BDMA : Allocate an array to store adc values to SRAM4.In all experiments, the correct value do...

ssooki by Associate III
  • 3132 Views
  • 4 replies
  • 0 kudos

Resolved! Is it safe to use +5 volts for I2C with this MPU?

I'm using a Portenta H7 from Arduino. It hosts the STM32H747 microprocessor. I was wondering if it is safe to use +5 volts for I2C even though the MPU runs at +3.3 volts? To clarify, on how the Portenta H7 is wired up, I'm using the pins associated w...

0693W00000FC7VUQA1.png
JChan.12 by Associate II
  • 4552 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L562CET6 won't enter EXTI callback function.

I am quiet new to STM32 programming and can't get the external interrupt to work.I started with the NUCLEO-L011K4 and wrote my programm without any issues. I switched to my own board (pdf included) and weren't able to get extrenal interrupts to work....

LOlhe.1 by Associate II
  • 13107 Views
  • 12 replies
  • 0 kudos

ADC

Hi All,I would like to configure my ADC such that it is able to read from 2 channels. And that the conversion of the channels will be stored in the memory through DMA. But most importantly, I want the conversion to be triggered by a TIMer's rising/fa...

STM32H743 out of sequence packet issue

HI,I am using stm32h743 controller and trying to port http webserver application which was working on stm32f7 platform. the application is using socket based apis. here i am generating the code using stm32cubeMX with STM32Cube_FW_H7_V1.9.0 package. A...

When exactly does SPI TXE get set in an F730

I am trying to change from using a Timer PWM controlled outgoing bit stream to an SPI controlled outgoing bit stream. It would be very nice to output a 32-bit word in one shot using the 4-byte FIFO at each TXE interrupt, but the RM seems to indicat...

GLero.1 by Associate II
  • 2988 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.