2021-09-30 11:17 PM
I read the adc value using ADC3 + DMA using STM32H725.
ADC3 channel 0,1,10,11 are reading adc value.
1) ADC3 + DMA1 : RAM 0x24000000 ~ 0x2401FFFF
2) ADC3 + BDMA : Allocate an array to store adc values to SRAM4.
In all experiments, the correct value does not come out, but 0 or a very large value comes out, and even if the power of the corresponding channel is cut off, a strange value comes out...
What more should I consider and test?
The structure of H7 is complicated, so there are too many things that I don't understand because of my short knowledge... Please explain in detail.
2021-10-01 8:24 AM
If the value is getting populated, the DMA is probably putting it there, barring any rogue out of bounds accesses.
Get the ADC working in blocking mode first. Plenty of examples to go off of.
2021-10-03 6:11 PM
2021-10-04 8:51 AM
Hi @ssooki ,
Some explanation of DMA weird behavior with STM32H7 in this article: DMA is not working on STM32H7 devices.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-10-12 3:17 AM
Hello @ssooki ,
For the setup "ADC3 + DMA1": Can you start from an example of FW package, for example:
...\Firmware\Projects\NUCLEO-H743ZI\Examples\ADC\ADC_DMA_Transfer
with modifications:
Best regards
Philippe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.