STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G474 boots with FPU enabled when BFB2=1

We are using the STM32G474 MCU in dual-bank mode. In the options registers we have DBANK=1 and BFB2=0 or 1 depending on which bank we are booting from at the moment (we swap banks during firmware updates). We have found that when booting and BFB2=0 t...

Resolved! Working of RTO (receiver timeout) in UART?

Hello,I have been looking into this RTO flag provided in STM32F303 UART.According to the manual"The timeout function and interrupt must be activated, through the RTOEN bit in the USART_CR2 register and the RTOIE in the USART_CR1 register. The value c...

Sdddd by Associate II
  • 15018 Views
  • 10 replies
  • 0 kudos

STM32F4 using DMA and ADC with LL

Hello, I'm working with a nucleo F401RE board and the LL drivers, I have set up the ADC in DMA mode, checking into the DMA register all seems right, but when I start the ADC it converts only one value and than it stop, the ADC is triggered from an EX...

CCont.3 by Associate
  • 4824 Views
  • 3 replies
  • 0 kudos

Unreadable flash due to power failure

We met with strange problem with STM32H743. Could you please advice how to diagnose the following bug/effect of built-in flash :we use STM32H743 at our device. We calibrate the device within assembling procedure. The calibration data stored in built-...

AVlad.1 by Associate II
  • 3338 Views
  • 5 replies
  • 0 kudos

STM32U5 GPDMA

Hi,The GPDMA of the STM32U5 is much more complex to configure than the DMA of the other STM32. I would like to know in which applications GPDMA is better than DMA and also would like to know if ST has plans to use GPDMA in future general purpose micr...

AMend.5 by Associate III
  • 2356 Views
  • 3 replies
  • 0 kudos

Resolved! What Can I do for solve this error? I refer to this GitHub! https://github.com/jrmejiaa/ESP8266 char *arg[CountOfParameter]; <-- this part makes error

#include "ESP8266.h" #include "ESP8266Config.h"   //######################################################################################################### bool Wifi_SendRaw(uint8_t *data,uint16_t len) { if(len <= _WIFI_TX_SIZE) { // Send the i...

0693W00000FDF8GQAX.png
wwgww by Associate II
  • 1515 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G473CB Flash Bank Configuration

I'm currently trying to implement the eeprom emulation library provided by ST on an STM32G473CB. However, I'm dubious about whether this library, and also the HAL flash modules, are properly detecting that I'm working with this specific device.From w...

schwil by Associate II
  • 2501 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.