Ask questions, find answers, and share insights on STM32 products and their technical features.
Part Number: STM32F091VBPart Family: STM32F091xxQuery Description:From the datasheet of STM32F091VB, the current IDD_VBAT through the VBAT Pin is noted as belowThe data in the above table is given in the condition where LSE and RTC in ON.In our appli...
You can't reprogram flash double words on the stm32g4 even if the were programmed to 0xFFFF'FFFF'FFFF'FFFF.Does anyone know if it is possible to check if the 0xFFFF'FFFF'FFFF'FFFF value I read from a specific flash position has previously been progr...
I look at SR2 PEC contents (most significant 8 bits), and they always are zero. Is that normal?
Hello, I work on a project using SPI to communicate Data acquired and processed with Motion FX. When an incomming signal is received, i want to reset my STM32 MCU with a software reset. However, when i do so using NVIC_SystemReset(), the spi communic...
I am trying to use IDB05A1 BLE module in low power mode with STM32L073RZ MCU. I didn't get any reference for doing it without the DMA.
I couldn't find within the data sheets whether the chip suffix, 3 or 6, which indicates temperature range, is programmed in the chip. This might help to set temperature alerts at the right level.Does it exist?
I'm using the below to calculate the temperature in STM32L452 CPU:int16_t temperatureC ;// ADC VREF is external 3V3temperature = __HAL_ADC_CALC_TEMPERATURE (3300, ADC_val, ADC_RESOLUTION_12B);For ADC_val = 1360 - then temperatureC is 164 Celsius, whi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.