STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I work this process minimum 750 Hz in Nucleo L432?

Hello. For a project, I need to read 4 channels analog data and save them in to the sd card for 10 seconds. I should record every data minimum with 750 Hz. And then I generate pwm signal with these data. I tried that but it was not successful, recor...

MÇeli.2 by Associate II
  • 1863 Views
  • 3 replies
  • 0 kudos

DMA vs BDMA

HiI want to use spi6 on stm32h7 controller in DMA mode, i see i can use BDMA instead of DMA. looking at the reference manual, i see following about BDMA"The BDMA is used to perform programmable data transfers between memory-mapped peripherals and/or ...

DGupt by Associate III
  • 8159 Views
  • 4 replies
  • 0 kudos

Resolved! High-frequency square wave using timer not possible?

Hi,I'm trying to see what the maximal frequency I can achieve using the STM32F407-discovery board.So far I have found the following:using TIM1 Internal clock (168MHz)Output pin PE9If i put the period at 1000, I get the following result:However if I p...

0693W00000FDmVmQAL.png 0693W00000FDmW1QAL.png
MDrac.1 by Associate III
  • 16102 Views
  • 4 replies
  • 0 kudos

Resolved! openOCD not reseting my chip :_(

Trying to build my own raspberryPi wireless SWD debugger.(bitbanging SWD, without stlink)I am able to flash and halt the code trough cubeIDE but openOCD is not able to reset the chip, i have to do it manually for now (see gif above).Pesky errors im g...

0693W00000FDmMGQA1.gif 0693W00000FDmFZQA1.png 0693W00000FDmFKQA1.png
Javier1 by Principal
  • 9776 Views
  • 6 replies
  • 1 kudos

STM32L552: DP TARGETID reads 00000001

Hello,with the same procedure that reads the DP TARGETID fine on STM32F7 and STM32H7, on STM32L5 the TARGETID only reads 00000001 (RM0438, p 2000, DP target identification register (DP_TARGETIDR).Do I do something wrong or is this an errata not yet l...

STM32F439 power down GPIO state

When STM32F439 power supply is dropping from 3.3V to 0V what will be state of GPIO which is configured as Mode output pp, pull up and speed_fast whether it will hold to value mentioned in GPIOx_ODR

PV C by Associate II
  • 1046 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.