2021-12-07 6:35 AM
Hello.
The project I am actually working on uses several peripherals such as USART ADC SPI etc.
I am trying to use as much DMA as I can, but there is something that I miss in the reference manual and on the internet.
Can I use ONE channel with TWO streams of TWO independant IPs ?
Can I use ONE channel with TWO streams of ONE IP ?
For instance with a STM32F427:
UART4 uses dma1 stream2 with channel4 and dma1 stream4 with channel 4
and
USART2 uses dma1 stream6 with channel4 and dma1 stream0 with channel 4
In this example :
Could I use the two streams for UART4 or only one stream at a time ?
Could I use every streams that I quoted for UART4 and USART2 (D1S2C4, D1S4C4, D1S6C4 and D1S0C4) at the same time ?
Thank you,
Have a nice day.
2021-12-07 6:59 AM
There is no restriction on using the same channel on multiple independent streams.
You can't use multiple channels within a single stream, and you can't have the same request mapped to multiple streams.
2021-12-07 8:19 AM
"Stream" in the DMA in 'F4 is one element of the DMA which performs the transfer.
"Channel" is only the setting of a stream's request multiplexer.
Read the DMA chapter in RM0090.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.