STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC conversion triggered by timer output compare

I am trying to make the ADC channels sample the current through some motor channels synchronised to the center of the center aligned PWM waveform to avoid switching noise.The microcontroller I am using is the STM32F411 series, and I am using the firs...

eggsacc_0-1755228333971.png eggsacc_1-1755228352332.png eggsacc_2-1755228390909.png
eggsacc by Associate II
  • 1648 Views
  • 1 replies
  • 0 kudos

STM32533RE - programming with nucleo ST-link

Hi,Could someone be so kind as to explain in ***-proof terms exactly how I would connect an ST-link from a nucleo board to a custom STM32533RE PCB so that it can be programmed and debugged with STM32CubeIDE?  Which pins from the MCU do I need to make...

STM32F103 usb data loss

I'm trying out a test program to measure data rate between pc and mcu over usb.I'm using winusb with winusbnet wrapper on pc side and for mcu firmware i followed this github repo https://github.com/MichaelTien8901/STM32WINUSBto get it built with winu...

MMala.3 by Associate II
  • 901 Views
  • 4 replies
  • 1 kudos

F767 USB DFU - upload firmware

Hello... i am design a board based on STM32F767 using USB to upload and upgrade firmware i.e. USB DFU could anyone advise any EVK or schematic daigram for USB to STM32F767 ? Pls advise soon. 

Resolved! F767: USB Device DFU crystal 8 MHz

Hello.. Anyone can advise if using USB Device for DFU, which crystal should i use? 25MHz? Why i dun see the 25 MHz crystal on 767 Nucleo ?  if i only include the 8 MHz crystal (as the main clock )is it fine to drive the USB Device DFU? Please advise?...

STM32H573VIT3Q Programming Issues

We are using the STM32H573VIT3Q in our project and have developed a POC board.While programming via STM32CubeIDE in debug mode, we are encountering random errors (refer to the attached screenshots).Additionally, STM32CubeProgrammer is detecting the c...

Abhijeet4 by Associate II
  • 1261 Views
  • 4 replies
  • 0 kudos

Unused pin on STM32F767

Hello.. i m designing a board using STM32F767, could anyone advise what should be done to those unused pins? Ground it or set it to ERC on Altium? 

STM32G071CBT6TR- New Carrier Tape consult

Dear all, Recently, when we were using STM32G071CBT6TR, we discovered some IC bent leads issues. At present, we have not found IC bent leads issues in the original packaging.We are investigating the risk points. Meanwhile, we have also checked the PC...

weihu by Associate
  • 493 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.