2025-08-04 7:02 PM
Hello... i am design a board based on STM32F767 using USB to upload and upgrade firmware i.e. USB DFU could anyone advise any EVK or schematic daigram for USB to STM32F767 ? Pls advise soon.
2025-08-05 3:13 AM
You can find schematics under cad resources, schematics pack for Nucleo F767ZI.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-13 8:04 AM
Hello.. Anyone can advise if using USB Device for DFU, which crystal should i use? 25MHz? Why i dun see the 25 MHz crystal on 767 Nucleo ?
if i only include the 8 MHz crystal is it fine to drive the USB Device DFU? Please advise?
2025-08-14 3:15 AM
Indeed it should be ok, here is an example provided using the same board in device mode,
Regarding your second question, when using an 8 MHz HSE, it is mentioned in the datasheet that the USB OTG controller requires a dedicated 48 MHz clock, which is generated by a PLL connected to the HSE oscillator. There is no restriction on the source, as the PLL multipliers can achieve a 48 MHz clock source to feed the USB peripheral.
If your questions are answered, click on Accept as Solution.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-14 3:28 AM
Doesn't AN2606 state the accepted crystal frequencies?? Pretty sure 8 or 25 MHz meet requirements..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.