STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 Disco with HM-10

Hello! I just got the STM32F429 Disco board and I'm trying to connect it to the HM-10 bluetooth module. I'm completely out of my depth here, I was hoping someone could nudge me in the right direction.I've worked with the HC-05 and the HM-10 on the ar...

BBrus.1 by Associate
  • 2723 Views
  • 1 replies
  • 0 kudos

There is no DWT in the M0/M0+ kernel.

Hi. I am using stm32l01c6tx. I want to use a very simple microsecond function. Libraries I have added below. "DWT" "CTRL" etc. when I included the libraries. It says not defined. But they are all in the "core_cm4.h" library. This library is in Driver...

ZKURT.1 by Senior
  • 10117 Views
  • 8 replies
  • 0 kudos

Resolved! Error on Application note (AN2834), AND Where to report it?

In application note AN2834 (How to get the best ADC accuracy in STM32 microcontrollers), There is a clear error on Page 10, which defines 1 LSB by Vref+/2^12). But LSB depends on Resolution!If Resolution is 10, then it would be defined by Vref+/2^10....

0693W00000Dq1CsQAJ.png
Ass.1 by Associate
  • 2995 Views
  • 3 replies
  • 1 kudos

Vbat pin drawn high currebt when power is off

I am using Nucleo 144 H745ZQi , connected vbat pin directly using coin cell, when power is off/unconnected, LD7 led ovcr indicator turned on and current consumption drawn from baterry was 50mA, also the LD5 led turned on. However when i reconnect the...

SJati.1 by Associate II
  • 14015 Views
  • 14 replies
  • 0 kudos

DMA Uart Rx occur only once

I have followed an example found on the web to get DMA RX usart2 running.I had activate RX DMA, global interrupt in cubmx project.In the main I have :HAL_UARTEx_ReceiveToIdle_DMA(&huart2, RxBuf, RxBuf_SIZE); __HAL_DMA_DISABLE_IT(&hdma_usart2_rx, DM...

MGuil.1 by Associate II
  • 6804 Views
  • 10 replies
  • 0 kudos

HAL_Delay / HAL_SuspendTick ?

I am trying to run code in LPSleep mode. I found a video that seems to describe the use of SuspendTick and ResumeTick to do this. I have created a small example where I push a button it jumps into an EXTI handler and toggles an LED. Within this IS...

0693W00000HoqyQQAR.png 0693W00000HoqyLQAR.png
SWenn.1 by Senior III
  • 4006 Views
  • 3 replies
  • 0 kudos

LPTIM -- 50ms debounce measuring 62ms ???

I have a scope and am triggering on the falling edge of a pushbutton. The LED drive signal is being monitored on another scope channel. The LED is to turn on 50ms after the falling edge of the pushbutton but in reality it is 62ms. LPTIM1 is runnin...

SWenn.1 by Senior III
  • 1623 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.