2021-12-19 11:09 PM
Hi,
I am working on STM32G071RB Nucleo Board and In one of project , I am using same MCU.
In that Project , I don't want to use external I2C or SPI memory for saving the data (logs).
1) How do I can access Flash as EEPROM ?
2) Will this possible with STM32Cube MX ?
3) How the EEPROM Locations (Say 100 Bytes) are separated from Flash Memory Content (Actual Program) ?
Thanks in Advance
--
Karan
2021-12-19 11:37 PM
Check the AN4894 Application note "EEPROM emulation techniques and software for STM32 microcontrollers" and the X-CUBE-EEPROM library.
hth
KnarfB
2021-12-20 5:40 AM
Hi @KnarfB ,
Thanks for Update. I have already seen that Application Note and X-CUBE-EEPROM library.
I am trying to use that (add) Library in my existing project (EEPROM_Emul Folder)
But facing below issue eeprom_emul.h .
../Core/Src/main.c:27:10: fatal error: G:\STM32G0 Cube\Dec 2021\Single Timer - 2\BlinkingG0\EEPROM_Emul\core\eeprom_emul.h: No such file or directory
#include "G:\STM32G0 Cube\Dec 2021\Single Timer - 2\BlinkingG0\EEPROM_Emul\core\eeprom_emul.h"Please check attach code using that library.
Thanks for your concern..
--
Karan
2021-12-20 7:19 AM
The compiler says it can't find that file, does that file exist on the drive?
Usually relative directories are used for include files.
2021-12-20 8:42 AM
Hi TDK,
Thanks for update..
1) Have to check attached project.. ?
2) eeprom_emul.h is already present inside the EEPROM_Emul Folder ?
-Usually relative directories are used for include files.
Can you help to compile this attached project..?
--
Karan
2021-12-21 2:56 AM
Spaces in the path. "G:\STM32G0 Cube\Dec 2021\Single Timer - 2\....."
This can cause all kinds of nasty things.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.