STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C Master Sequential function

Dear,I currently use a STM32G070 with external touch sensor component usuing I2C interface.This component aloow me to communicate with it only during a ready window and this window is automatically closed after a delay without communication or a I2C ...

0693W00000JPpzuQAD.png
YDann.7 by Associate III
  • 6755 Views
  • 5 replies
  • 0 kudos

Can sdio f_mount affect UART port?

Hi!I have a problem with the simultaneous use of an SD card (with SDIO) and the uart port with GSM module connected. The SD card works flawlessly all the time. Communication with the GSM module is very unstable when I use the SD card - using the f_mo...

STM32G031xx: Mistake/Bug in device specific header file???

Hiso I am trying to get the UART2 on my STM32G031K8Tx up and running. RefManual shows in Chapter 5.4.21 a CCIPR register (Peripherals independent clock configuration register), where bits 2-3 relate to the USART2.When looking at the device specific h...

AAnth.1 by Senior
  • 2601 Views
  • 4 replies
  • 0 kudos

Hi. I boot with stm32L010C6Tx. I am in standby mode. While waiting in standby mode, it shows between 3.1 micro amps and 50 micro amps 50 microamps is too high, I can't use it like this. . I turned off all peripherals. What else should I turn off? Why coul

void SystemClock_Config(void);static void MX_GPIO_Init(void);static void MX_LPUART1_UART_Init(void);static void MX_I2C1_Init(void);static void MX_ADC_Init(void);static void MX_RTC_Init(void);if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET) { __HAL_PWR_...

ZKURT.1 by Senior
  • 1511 Views
  • 2 replies
  • 0 kudos

Trigger SPI Read using Timer Update Event

Hello,I am trying to trigger each DMA read of my SPI to happen on update event Trigger output of my Timer but I don't think I have it setup correctly.I've seen this done using the internal ADC, where you can set the external conversion trigger source...

kcire L. by Associate III
  • 3604 Views
  • 3 replies
  • 0 kudos

Max voltage on pins when unpowered?

Hello,I notice in the STM32G030x6/x8 datasheet, Table 18 that the max input voltage on FT_xx and any other pin are VDD + 4V and 4V respectively. Does this mean those pins can be safely driven with 3.3V when the MCU is unpowered?Thanks,Nicholas

NLuon.3 by Associate
  • 1308 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.