STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RTC Reference Clock (50Hz) worsens the LSE accuracy

As indicated by an4759, I am trying to use the 50Hz mains reference to improve the RTC accuracy of an STM32F413ZH.However, the results I get are much worse than without using the reference:LSE only: 0.6s/dayLSE+50Hz: 7.5s/day (test duration 4 days)Ac...

0693W00000JPqz8QAD.png 0693W00000JPr5FQAT.jpg 0693W00000JPr8JQAT.jpg 0693W00000JPr8sQAD.jpg

Incomplete HAL_DMA_Abort_IT() in STM32F7xx_HAL v1.16

Hello,During a UART transfer I used the HAL_DMA_Abort_IT() function. The transfer stopped but the DMA handle stays locked and in the HAL_DMA_STATE_ABORT. When in this state the only thing to do is reinitialize the peripheral.Anyone have some feed bac...

ibobbymk by Associate
  • 745 Views
  • 0 replies
  • 0 kudos

ADC on ST Nucleo H743ZI board with DMA on Zephyr platform.

Hai, I am working with ST Nucleo H743ZI board for analog-to-digital conversion without CPU intervention between samples, by using DMA in Zephyr platform. Is there any ready-made example for the above, that I can refer?Thank you. Sachin

SJ.7 by Associate
  • 804 Views
  • 0 replies
  • 0 kudos

I have question on STM32F777 RTC and super cap

I wanted to use RTC Circuit for Supercap.I have designed circuit (Check Attached snapshot).but i dont get back up time? can anyone explain do we need to do any provision in controller.It seems that capacitor is discharging very fast

0693W00000JPlkbQAD.jpg
Chiku by Associate II
  • 2016 Views
  • 3 replies
  • 0 kudos

Odd glitch experienced on STM32F7 TIM8 PWM. - FIXED

I am seeing a very strange glitch from the PWM output of TIM8:CH1 on an STM32F730.The timer is running on 216MHz internal clock, with an ARR reload of 617, giving a ~350kHz PWM output.There is also a no-output Compare on it's channel 2, used to trigg...

0693W000001ptqKQAQ.png
EdGi by Associate III
  • 4235 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.